This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: SPI从机模式下触发SPI_TRANSFER_CANCELED问题

Part Number: CC1310


你好 关于CC1310芯片的SPI从机的使用的一些问题需要咨询

本程序下使用SPI从机时钟为4M,模式为如下

现出现在使用过程中SPI主机以5ms左右时间通信一次,数据量在1024字节,不定时出现SPI_TRANSFER_CANCELED状态是什么问题?

目前观察simplelink_cc13x0_sdk_4_20_02_07\source\ti\drivers\spi\SPICC26XXDMA.c文件看到由cs管脚会出现这个状态,但是目前SPI未配置cs管脚,还有哪里会触发“传输取消”这个状态?

以及ti库有单步调试方法吗?