什么是loopback connection 有相关资料吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
sensortag的代码里面的 谢谢
static void gyro_HandleConnStatusCB( uint16 connHandle, uint8 changeType )
{
// Make sure this is not loopback connection
if ( connHandle != LOOPBACK_CONNHANDLE )
{
// Reset Client Char Config if connection has dropped
if ( ( changeType == LINKDB_STATUS_UPDATE_REMOVED ) ||
( ( changeType == LINKDB_STATUS_UPDATE_STATEFLAGS ) &&
( !linkDB_Up( connHandle ) ) ) )
{
GATTServApp_InitCharCfg( connHandle, gyroDataConfig );
}
}
发送的数据被接收端回送回来,被称为loopback. 用于检测连接问题,从程序上看0XFFFE被作为一个特殊的connHandle。这个应该是底层用于测试目的的。