This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2500问题:

1. 发纯载波,怎么做?

2. GDO0 始终无法正常工作(主设备GDO0输入模式正常,我是没招了,希望这儿能得到答案!)

寄存器配置如下:

 spi_write_reg(CCxxx0_IOCFG2, 0x29);    //  GDO2 output pin config.

 spi_write_reg(CCxxx0_IOCFG0, 0x06);    //  PIN_GDO0 output pin config.
 
 spi_write_reg(CCxxx0_PKTLEN, 0xff);    // 06 Packet length.
 spi_write_reg(CCxxx0_FSCTRL1, 0x12);    // 0b  Freq synthesizer control.
 spi_write_reg(CCxxx0_FSCTRL0, 0x00);    // 0c  Freq synthesizer control.
 spi_write_reg(CCxxx0_PKTCTRL1, 0x04);    // 07 Packet automation control.
 spi_write_reg(CCxxx0_PKTCTRL0, 0x05);    // 08 Packet automation control.

 spi_write_reg(CCxxx0_CHANNR, 0x00);    // 0a  Channel number.
 
 spi_write_reg(CCxxx0_FREQ2,  0x5d);    // 0d  Freq control word, high byte.
 spi_write_reg(CCxxx0_FREQ1,  0x93);    // 0e  Freq control word, mid byte.
 spi_write_reg(CCxxx0_FREQ0,  0xb1);    // 0f  Freq control word, low byte.
 spi_write_reg(CCxxx0_FSCAL3, 0xea);    // 23  Frequency synthesizer cal.
 spi_write_reg(CCxxx0_FSCAL2, 0x0a);    // 24  Frequency synthesizer cal.
 spi_write_reg(CCxxx0_FSCAL1, 0x00);    // 25  Frequency synthesizer cal.
 spi_write_reg(CCxxx0_FSCAL0, 0x11);    // 26  Frequency synthesizer cal.
 spi_write_reg(CCxxx0_FSTEST, 0x59);    // 29  Frequency synthesizer cal.
 
 spi_write_reg(CCxxx0_MDMCFG4, 0x2d);    // 10  Modem configuration.
 spi_write_reg(CCxxx0_MDMCFG3, 0x3b);    // 11  Modem configuration.
 spi_write_reg(CCxxx0_MDMCFG2, 0xf3);    // 12  Modem configuration.
 spi_write_reg(CCxxx0_MDMCFG1, 0x22);       // 13  Modem configuration.
 spi_write_reg(CCxxx0_MDMCFG0, 0xf8);    // 14  Modem configuration.
 spi_write_reg(CCxxx0_DEVIATN, 0x00);    // 15  Modem dev (when FSK mod en)
 spi_write_reg(CCxxx0_FREND1, 0xb6);    // 21  Front end RX configuration.
 spi_write_reg(CCxxx0_FREND0, 0x10);    // 22  Front end RX configuration.
 
 spi_write_reg(CCxxx0_FOCCFG, 0x1d);    // 19  Freq Offset Compens. Config
 spi_write_reg(CCxxx0_BSCFG,  0x1c);    // 1a  Bit synchronization config.
 spi_write_reg(CCxxx0_AGCCTRL2, 0xc7);    // 1b  AGC control.
 spi_write_reg(CCxxx0_AGCCTRL1, 0x00);    // 1c  AGC control.
 spi_write_reg(CCxxx0_AGCCTRL0, 0xB0);    // 1d  AGC control.
 spi_write_reg(CCxxx0_MCSM1,  0x3f);    // 17  MainRadio Cntrl State Machine
 spi_write_reg(CCxxx0_MCSM0,  0x18);    // 18  MainRadio Cntrl State Machine

 spi_write_reg(CCxxx0_TEST2,  0x88);    // 2c  Various test settings.
 spi_write_reg(CCxxx0_TEST1,  0x31);    // 2d  Various test settings.
 spi_write_reg(CCxxx0_TEST0,  0x0b);    // 2e  Various test settings.
 spi_write_reg(CCxxx0_FIFOTHR, 0x07);     // FIFOTHR   RXFIFO and TXFIFO thresholds.
 
 spi_write_reg(CCxxx0_ADDR,  0x00);    // 09 Device address.

 

1.zip