This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7960A 在ISO15693协议下1出256低速率双副载波的问题,可能是芯片固件BUG



1、使用TRF7960AEVM读取ISO15693协议标签;

2、设置读写器通信速率为1出256,发送Flag = 01h的命令(低速率双副载波),所有命令均收不到标签响应。

3、使用示波器抓取天线场的波形发现,读写器调制完SOF后,在调制Flag = 01h数据的脉冲调制在了前9.44us,也就是01h数据变成了EOF标志了!!!为什么?

4、修改程序,在设置ISO Control寄存器后(设置为低速率双副载波1出256),不对TX Pulse width寄存器进行设置(或者设置为0);使用示波器抓取天线场内波形,发现Flag = 01h调制脉冲宽度变成了18.88us了,后续字节调制正常。改变ISO Control寄存器为其它值,调制脉宽均为9.44us。

5、使用TRF7960AEVM开发板,程序为官方程序;上位机软件使用官方Demo程序,发现同样的问题。

希望能有专家尽快给我回复,是不是芯片固件的BUG,如何能避免这个问题?目前项目都到了最后集成测试阶段了!!!万分火急,希望能与我联系,邮箱:zhangqq@hed.com.cn;电话18610594002.

谢谢!!!!不胜感激