This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1101通信距离

Other Parts Discussed in Thread: CC1101

做的好的话cc1101在5db的通信距离大概各能达到多少?433MHZ,100K的通信速度.

  • 您好,影响通信距离的几点重要因素:1.电路匹配;2.天线的方向性;3.输出功率;4.接收灵敏度;5.外界环境。所以没有一个具体的数据提供给您,同时也可以使用PA增加发射功率,比如TI在1GHZ以下提供了CC1090.

  • 很多设计者都会对距离有一定疑问,个人觉得抛去应用环境谈距离是没有实际意义,433Mhz本身是sub 1G频段,其传输距离要好于2.4G的,但传输距离多远有很多因素觉得,天线的layout,发射功率/方向,测试环境等都会影响到传输距离,如果在设计的项目里很好满足了项目需求就可以。

  • 你如果需要更远的话,您可以加pa

  • 关键是你想要多远,我们用同样的板子有几百米的,有几十米的,环境不同,后有所改变的

  • 你好!

           我使用CC1101在433MHZ通信,开始至今使用TI提供实例里的配置,能正常通信,但发现通信距离只有20几米,然后将天线改为大功率天线,并增加了PA为C0,已经是比较大的PA了,结果通信距离还是没有得到改善,最后将数据率配置部分的寄存器修改配置为10K数据率,原配置为250K的数据率,结果直接不能通信,现在项目急切需要至少300米的通信,希望能得到您的宝贵建议,非常感谢!

  • 你好!

           我使用CC1101在433MHZ通信,开始至今使用TI提供实例里的配置,能正常通信,但发现通信距离只有20几米,然后将天线改为大功率天线,并增加了PA为C0,已经是比较大的PA了,结果通信距离还是没有得到改善,最后将数据率配置部分的寄存器修改配置为10K数据率,原配置为250K的数据率,结果直接不能通信,现在项目急切需要至少300米的通信,希望能得到您的宝贵建议,非常感谢!