怎样设置CC1120的占用带宽(OBW)?
CC1120设置占用带宽的寄存器是不是CHAN_BW? 我们需要将占用带宽设置低于8.5KHz, Smart RF studio 设置RX filter BW 为8.333KHz,CHAN_BW 变为0x18. 但是我们用频谱仪测试时候(测试条件RBW:100HZ,VBW:100Hz,扫宽:50KHz,功率比99%)占用带宽为11KHz。 这里具体怎样设置占用带宽?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tx 端是通过设置 Deviation。 占用带宽 = 2 x Deviation。 但是在接收端Rx BW 需要大于 2x Deviation + 4 x Frequency Error (晶振误差带来的载波频率误差)。详情请参考 DN005。