This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 无线组网中的从机低功耗应用

Part Number: CC1310


老师们好,要开发一个无线组网的应用,主机长供电,若干个子设备使用电池供电,主机给某个子设备发命令后,子设备需要产生应答,尝试在rfSynchronizedPacketRx和 rfSynchronizedPacketTx上做修改,但子设备没有产生应答,请问有相关例程参考吗。主机发送,子设备应答,主机收到应答,满足这个过程就可以。谢谢。

  • 您好,

    建议您参看SimpleLink Academy中的 Sensor and Collector - TI 15.4-Stack Project Zero 会有手把手教程讲述相关您所想要开放的一个内容。

    以下为该实验的一个内容和目标:

    In this lab, we will run a pair of examples based on the complete TI 15.4-Stack, one Sensor and one Collector - creating a star network of sensor node(s) sending data to a collector.

    • The Collector Example Application implements the PAN-Coordinator, or the central node in the network. This application starts the network, allows devices to join the network, and configures the joining devices on how often to report the sensor data. It then sends periodic tracking request messages (to which it expects tracking response messages) to determine whether or not the sensor nodes are alive in the network.
    • The Sensor Example Application implements the networked device, which joins the network started by the Collector. The Sensor periodically sends sensor data reports at the report interval configured by the Collector and responds to the tracking messages it receives.
  • 谢谢您提供的资料,我先学习一下,有问题再来咨询

  • 您好,

    希望能够帮助到您,有问题您可以重新开帖提问,感谢您的支持。

    此贴将会关闭。