This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1110调试问题



各位大神求救,我调试CC1110的时候出现问题,求大神打救

Error[e16]: Segment ISTACK (size: 0x40 align: 0) is too long for segment definition. At least 0x2d more bytes needed. The 
problem occurred while processing the segment placement command 
"-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#08-_IDATA0_END", where at the moment of placement the available 
memory ranges were "IDATA:ed-ff"
   Reserved ranges relevant to this placement:
   IDATA:8-1f           IDATA_I
   IDATA:21-62          IDATA_I
   IDATA:63-ec          IDATA_Z
   IDATA:ed-ff          ISTACK
   BIT:0-7              BREG
   BIT:88-9f            SFR_AN
   BIT:a8-af            SFR_AN
   BIT:b8-c7            SFR_AN
   BIT:d8-df            SFR_AN
   BIT:e8-ef            SFR_AN