This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PurePath无线开发套件master和slave两方是否需要采用同样的音频编解码器才能成功传输



我使用了PurePath无线开发套件,master使用CC8532+AIC3101采用的是无线开发套件板子原有的所有硬件,而slave方则使用了AIC3254编解码器来替代AIC3101,因此在slave这采用了CC8532+AIC3254. 结果是不能完成音频的无线传输。我想问的是,是不是必须maste和slave两边必须使用同样的编解码器才能完成无线音频传输。因为在slave这边用原有的AIC3101可以听到master传来声音,但是换成AIC3254后就不行了。希望工程师给出解答,谢谢!