最近在使用DP83848I和stm32连接,发现参考电路上RMII接口都串行了一个33欧姆的电阻,这个电阻不知道有什么作用。在MII和RMII中有哪些线需要连接,MDC和MDIO线需不需要要连接,RMII中的共用50M的CLK需不需要接?如果这些线都需要连接的话,那电阻在PCB上的放置位置有没有要求,是更靠近DP83848还是MAC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在使用DP83848I和stm32连接,发现参考电路上RMII接口都串行了一个33欧姆的电阻,这个电阻不知道有什么作用。在MII和RMII中有哪些线需要连接,MDC和MDIO线需不需要要连接,RMII中的共用50M的CLK需不需要接?如果这些线都需要连接的话,那电阻在PCB上的放置位置有没有要求,是更靠近DP83848还是MAC?
Yanlong,
感谢您的配合!
另外您也可以到我们的E2E论坛中的Interface板块看看,里面会有更多关于DP83848产品的讨论.
链接如下:http://e2e.ti.com/search/default.aspx#q=DP83848&g=77
谢谢!
没有仔细看这两颗芯片的设计。不过一般这种高速接口的数据线串电阻是为了匹配阻抗,防止 Ringing(振铃),维护信号完整性。