小弟在测试基于CC1101在434频段的系统,测试发现6信道的传感器节点收发数据时,2信道的节点会产生中断(中断led闪烁),测试时只开启了6信道和2信道的节点,6信道节点是组成的无线网络,2信道只开启节点。通过频谱分析仪测试信道频率都设置正确,我的频率寄存器配置为:#define SMARTRF_SETTING_FREQ2 0x10 #define SMARTRF_SETTING_FREQ1 0xB1#define SMARTRF_SETTING_FREQ0 0x3B,信道间隔为199.9K。目前需要大规模组网,这个问题会严重干扰我们的进度,希望各位前辈能帮助给些意见,不甚感激!!!