This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 数据包传输时间过长

Part Number: CC1310


你好,

   我现在基于TI 15.4中的collector与sensor例程,想通过sensor向collector每一秒发送包含一百个ADC数据的数据包,但是我发现在实际传输过程中,数据包传输时长远远大于一秒钟,所以,我想询问一下有无对应的解决办法。

谢谢!

  • 您好,方便把发送数据包的代码发到这边吗?

  • 感谢您的回复!

    我在Sensor 部分中我将原来发送温度数据部分替换成发送100个ADC数据,在代码中可以看到,下面是sensor向collector发送数据部分的代码,数据可以成功发送,但是就是两次发送的时间间隔太长了,完全无法满足项目需求。

    static void processSensorMsgEvt(void)
    {
    Smsgs_sensorMsg_t sensor;
    uint32_t stat;

    memset(&sensor, 0, sizeof(Smsgs_sensorMsg_t));

    ApiMac_mlmeGetReqUint32(ApiMac_attribute_diagRxSecureFail, &stat);
    Sensor_msgStats.rxDecryptFailures = (uint16_t)stat;

    ApiMac_mlmeGetReqUint32(ApiMac_attribute_diagTxSecureFail, &stat);
    Sensor_msgStats.txEncryptFailures = (uint16_t)stat;

    ApiMac_mlmeGetReqArray(ApiMac_attribute_extendedAddress,
    sensor.extAddress);

    /* fill in the message */
    sensor.frameControl = configSettings.frameControl;
    if(sensor.frameControl & Smsgs_dataFields_tempSensor)
    {

    memcpy(&sensor.tempSensor, &tempSensor,
    sizeof(Smsgs_tempSensorField_t));
    }
    if(sensor.frameControl & Smsgs_dataFields_lightSensor)
    {
    memcpy(&sensor.lightSensor, &lightSensor,
    sizeof(Smsgs_lightSensorField_t));
    }
    if(sensor.frameControl & Smsgs_dataFields_humiditySensor)
    {
    memcpy(&sensor.humiditySensor, &humiditySensor,
    sizeof(Smsgs_humiditySensorField_t));
    }
    if(sensor.frameControl & Smsgs_dataFields_msgStats)
    {
    memcpy(&sensor.msgStats, &Sensor_msgStats,
    sizeof(Smsgs_msgStatsField_t));
    }
    if(sensor.frameControl & Smsgs_dataFields_configSettings)
    {
    sensor.configSettings.pollingInterval = configSettings.pollingInterval;
    sensor.configSettings.reportingInterval = configSettings
    .reportingInterval;
    }

    /* inform the user interface */
    Ssf_sensorReadingUpdate(&sensor);

    /* send the data to the collector */
    sendSensorMessage(&collectorAddr, &sensor);
    }

    static bool sendSensorMessage(ApiMac_sAddr_t *pDstAddr, Smsgs_sensorMsg_t *pMsg)
    {
    bool ret = false;
    uint8_t *pMsgBuf;
    uint16_t len = SMSGS_BASIC_SENSOR_LEN;

    /* Figure out the length */
    if(pMsg->frameControl & Smsgs_dataFields_tempSensor)
    {
    len += SMSGS_SENSOR_TEMP_LEN;
    }
    if(pMsg->frameControl & Smsgs_dataFields_lightSensor)
    {
    len += SMSGS_SENSOR_LIGHT_LEN;
    }
    if(pMsg->frameControl & Smsgs_dataFields_humiditySensor)
    {
    len += SMSGS_SENSOR_HUMIDITY_LEN;
    }
    if(pMsg->frameControl & Smsgs_dataFields_msgStats)
    {
    //len += SMSGS_SENSOR_MSG_STATS_LEN;
    len += sizeof(Smsgs_msgStatsField_t);
    }
    if(pMsg->frameControl & Smsgs_dataFields_configSettings)
    {
    len += SMSGS_SENSOR_CONFIG_SETTINGS_LEN;
    }

    pMsgBuf = (uint8_t *)Ssf_malloc(len);
    if(pMsgBuf)
    {
    uint8_t *pBuf = pMsgBuf;

    *pBuf++ = (uint8_t)Smsgs_cmdIds_sensorData;

    memcpy(pBuf, pMsg->extAddress, SMGS_SENSOR_EXTADDR_LEN);
    pBuf += SMGS_SENSOR_EXTADDR_LEN;

    pBuf = Util_bufferUint16(pBuf,pMsg->frameControl);

    /* Buffer data in order of frameControl mask, starting with LSB */
    if(pMsg->frameControl & Smsgs_dataFields_tempSensor)
    {
    for(int i=0;i<100;i++){
    pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.ambienceTemp[i]);
    }
    //pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.ambienceTemp);
    //pBuf = Util_bufferUint16(pBuf, pMsg->tempSensor.objectTemp);
    }
    if(pMsg->frameControl & Smsgs_dataFields_lightSensor)
    {
    pBuf = Util_bufferUint16(pBuf, pMsg->lightSensor.rawData);
    }
    if(pMsg->frameControl & Smsgs_dataFields_humiditySensor)
    {
    pBuf = Util_bufferUint16(pBuf, pMsg->humiditySensor.temp);
    pBuf = Util_bufferUint16(pBuf, pMsg->humiditySensor.humidity);
    }
    if(pMsg->frameControl & Smsgs_dataFields_msgStats)
    {
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinAttempts);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinFails);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.msgsAttempted);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.msgsSent);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.trackingRequests);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.trackingResponseAttempts);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.trackingResponseSent);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.configRequests);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.configResponseAttempts);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.configResponseSent);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.channelAccessFailures);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.macAckFailures);
    pBuf = Util_bufferUint16(pBuf,
    pMsg->msgStats.otherDataRequestFailures);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.syncLossIndications);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.rxDecryptFailures);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.txEncryptFailures);
    pBuf = Util_bufferUint16(pBuf, Ssf_resetCount);
    pBuf = Util_bufferUint16(pBuf, Ssf_resetReseason);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.joinTime);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.interimDelay);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.numBroadcastMsgRcvd);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.numBroadcastMsglost);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.avgE2EDelay);
    pBuf = Util_bufferUint16(pBuf, pMsg->msgStats.worstCaseE2EDelay);
    }
    if(pMsg->frameControl & Smsgs_dataFields_configSettings)
    {
    pBuf = Util_bufferUint32(pBuf,
    pMsg->configSettings.reportingInterval);
    pBuf = Util_bufferUint32(pBuf,
    pMsg->configSettings.pollingInterval);

    }

    ret = Sensor_sendMsg(Smsgs_cmdIds_sensorData, pDstAddr, true, len, pMsgBuf);
    if(ret == true){
    LCD_WRITE_STRING("Data Success Send", 2);
    }
    else{
    LCD_WRITE_STRING("Data Success Failed", 2);
    }

    Ssf_free(pMsgBuf);
    }

    return (ret);
    }

    Smsgs_tempSensorField_t修改后的结构

    typedef struct _Smsgs_tempsensorfield_t
    {
    /*!
    Ambience Chip Temperature - each value represents a 0.01 C
    degree, so a value of 2475 represents 24.75 C.
    */
    uint16_t ambienceTemp[100];
    /*!
    Object Temperature - each value represents a 0.01 C
    degree, so a value of 2475 represents 24.75 C.
    */
    //int16_t objectTemp;
    } Smsgs_tempSensorField_t;

    期待收到您的回复,非常感谢!

  • 好的,感谢您发过来的代码,我将需要一些时间来跟进您这边的问题。

  • 您是否调整了传感器的报告间隔?您的意思是,此消息本身的发送时间超过1秒吗?

  • 是的,我调整消息发送的时间间隔为一秒钟发送一次数据消息。具体代码如下所示:

    sensor部分关于时间的配置

    /*! Default Polling interval in milliseconds. It will get updated upon reception
    of a config request message */
    #define CONFIG_POLLING_INTERVAL 6000
    /*! PAN Advertisement Solicit trickle timer duration in milliseconds */
    #define CONFIG_PAN_ADVERT_SOLICIT_CLK_DURATION 6000
    /*! PAN Config Solicit trickle timer duration in milliseconds */
    #define CONFIG_PAN_CONFIG_SOLICIT_CLK_DURATION 6000
    /*! Default Reporting Interval - in milliseconds. It will get updated upon
    reception of a config request message */
    #define CONFIG_REPORTING_INTERVAL 1000
    #else
    /*! Default Polling interval in milliseconds. It will get updated upon reception
    of a config request message */
    #define CONFIG_POLLING_INTERVAL 60000
    /*! PAN Advertisement Solicit trickle timer duration in milliseconds */
    #define CONFIG_PAN_ADVERT_SOLICIT_CLK_DURATION 60000
    /*! PAN Config Solicit trickle timer duration in milliseconds */
    #define CONFIG_PAN_CONFIG_SOLICIT_CLK_DURATION 60000
    /*! Default Reporting Interval - in milliseconds. It will get updated upon
    reception of a config request message */
    #define CONFIG_REPORTING_INTERVAL 600000

    collector关于时间的配置

    /*!
    Reporting Interval - in milliseconds to be set on connected devices using
    configuration request messages
    */
    #define CONFIG_REPORTING_INTERVAL 90000
    /*!
    Polling interval in milliseconds to be set on connected devices using
    configuration request messages. Must be greater than or equal to default
    polling interval set on sensor devices
    */
    #define CONFIG_POLLING_INTERVAL 6000
    /*!
    Time interval in ms between tracking message intervals
    */
    #define TRACKING_DELAY_TIME 60000
    #else
    /*!
    Reporting Interval - in milliseconds to be set on connected devices using
    configuration request messages
    */
    #define CONFIG_REPORTING_INTERVAL 1000
    /*!
    Polling interval in milliseconds to be set on connected devices using
    configuration request messages. Must be greater than or equal to default
    polling interval set on sensor devices
    */
    #define CONFIG_POLLING_INTERVAL 60000
    /*!
    Time interval in ms between tracking message intervals
    */
    #define TRACKING_DELAY_TIME 300000

    我通过Csf_deviceSensorDataUpdate(&pDataInd->srcAddr, pDataInd->rssi,
    &sensorData);函数将数据打印出来,我发现在两块开发板写入程序,第一次上电时,ADC的数据可以通过串口一秒钟打印一次,但是出现“Configrap:0x1"后,两块开发板之间数据包的发送时常便变得比较缓慢了。

  • 好的,感谢您的回复,我这边会继续跟进。

  • collector关于时间的配置

    /*!
    Reporting Interval - in milliseconds to be set on connected devices using
    configuration request messages
    */
    #define CONFIG_REPORTING_INTERVAL 90000

    原来的时间配置错了,将这里的90000改成1000,现在可以实现一秒钟内完成数据的传输
    /*!
    Polling interval in milliseconds to be set on connected devices using
    configuration request messages. Must be greater than or equal to default
    polling interval set on sensor devices
    */
    #define CONFIG_POLLING_INTERVAL 6000
    /*!
    Time interval in ms between tracking message intervals
    */
    #define TRACKING_DELAY_TIME 60000
    #else
    /*!
    Reporting Interval - in milliseconds to be set on connected devices using
    configuration request messages
    */
    #define CONFIG_REPORTING_INTERVAL 1000
    /*!
    Polling interval in milliseconds to be set on connected devices using
    configuration request messages. Must be greater than or equal to default
    polling interval set on sensor devices
    */
    #define CONFIG_POLLING_INTERVAL 60000
    /*!
    Time interval in ms between tracking message intervals
    */
    #define TRACKING_DELAY_TIME 300000

  • 好的 我们这边也是考虑到这边的问题,很高兴能够帮助您解决问题,有问题欢迎来论坛交流学习,谢谢

  • 好的,非常感谢你们这段时间的持续关注。

    非常感谢!!!

  • 不客气,有问题随时论坛交流。时间可能会慢一点,但是一定会帮助您去解决问题的