您好!我再使用CC1352P7这个射频芯片设计产品时遇到如下问题:
1、正在使用CC1352P7设计一款产品,使用 +20dbm输出 Sub1G频段, +14dbm通路作为Sub1G作为接收通路,2.4G频段不使用,两个射频天线接口,一接口发射信号,另一接口接收信号,请问是否需可以不用射频开关?
2、如不使用射频开关,按照问题1描述,20dbm信号发射时,接收通路能接收到发送的信号,会不会损坏接收通道?
看着请回复,谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们仍然建议使用射频开关,以避免两条路径之间的相互作用。如果2.4 GHz路径未使用,则可以使用2端口开关,例如Richwave的RTC6608OU。
如果没有开关,RX端口仍然不会损坏。