This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101 250Kbps数据通信问题

Other Parts Discussed in Thread: CC1101, MSP430G2553

1、在进行通信测试时,采用可变长帧模式,最大长度为128B,GDO在接收状态配置为0x00,发送状态为0x02,当设置波特率在100Kbps(包含)以下时,通信正常。

2、但在250Kbps的空中速率下,数据长度超过90B的时候无法完成数据接收,仿真测试接收端是只处理了一次RxFIFO阈值超限事件,还未查到原因,请各位高人指教?

3、设置偏差为127K,接收带宽为540K,采用GFSK方式。

  • 请问是带 MCU 测的还是用 SmartRF Studio 测试的?什么MCU? 板子是用什么板子?TI的还是自己做的?

  • Nutcracker,你好!

    我用的MCU是msp430g2553,无线芯片用的是CC1101,自己设计的PCB。配置文件是通过SmartRF Studio生成的,通过TxFIFO和RxFIFO阈值实现128B可变长帧的发送和接收。现在问题是在无线波特率100Kbps(包含)以内时通信正常,在250Kbps速率下测试发现在数据帧长度不大于90个字节时通讯也很正常,但当大于90个字节后就无法完成接收。