您好:
我在WOR唤醒时,使能了RSSI监测功能, 根据AN047应用笔记上的说法,当没有检测到CS载波信号,就将进入Sleep睡眠状态,但是经过测量,我发现在没有监测到CS载波信号时,CC1101进入了Idle状态。等待整个事件的结束。这是为何???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我在WOR唤醒时,使能了RSSI监测功能, 根据AN047应用笔记上的说法,当没有检测到CS载波信号,就将进入Sleep睡眠状态,但是经过测量,我发现在没有监测到CS载波信号时,CC1101进入了Idle状态。等待整个事件的结束。这是为何???
RX 有个Timeout,之后就进入 Sleep 模式了。你的 Timeout 相关寄存器MSCM2.RX_TIME 和 WOR_RES 怎么设置的?Duty Cycle 是多少?你是通过看电流来判断Idle 还是 Sleep 吗?
首先我是通过电流来判断CC1101处于Idle状态和Sleep状态,Duty Cyle设置的是0.195%,我设置的WOR是1秒轮训。WOR_RES设置的为零。