eZ430-Chronos 手表套件里的CC1111 USB RF access point插在电脑上,然后打开SmartRF Studio 7,是不是应该能扫描到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你需要先连接CC Debugger 来 Program CC1111。
请参考 "eZ430-Chronos™ Development Tool User's Guide"。
3.6.3.4.1.2 Access Point Based on CC1111
The CC Debugger is required to program the CC1111 based RF access point. To perform the update, the
SmartRF Flash Programmer software is used to on the PC.
问一下WOR功能; 我设置IOCFG0.GDO0_CFG= 0x24;开始的时候很正常 GDO0引脚能检测到脉冲,并且电流有跳变,但是运行时间一长GDO0引脚有脉冲,但是电流保持1.7mA,应该是IDLE的功耗电流;请问有什么方法解决吗??
关于WOR功能,你是怀疑芯片一致在Idle状态,没到Sleep吗?
需要检查一下寄存器设置。
1.WOR 是否Enable?
2. 是采用的 MCSM2.RX_TIME_RSSI 还是 MCSM.RX_TIME检测?
3. 采用 TI 评估板对比测试一下。
另外新的问题最好单独发个帖子以提高可见度。