This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K 与电脑PING不通

Other Parts Discussed in Thread: DP83848K

采用的是RMII模式,采用AT91SAM9X35与DP83848,再加HR911105A的模式,原理如图

DP83848驱动采用公司原有的一般通用驱动,现在状态是用一般网线(公司其它项目用过,不知道是直连还是交叉,反正也是用DP83848可以PING通的)与我的电脑直连,就是PING不通(IP同一网段,子掩网一致)

原来的板子DP83848K有点发热,我看了下官方驱动电流为80MA(100M模式),焊了3块板子,测了2块,分别电流为91MA与110MA,今天重新焊了块,没测电流,但没有前两块热,所以应该没问题。

X1输出50M,TX_CLK与RX_CLK也是25M,所以晶振应该没有问题,同时电源波形也比较平滑。

以下是原理图及各个管脚波形,望帮我分析下。(电脑一直连续不断PING此板子时测的波形)

EMDC的波形

EMDI的波形

RXD0 的波形,RXD1的波形也差不多,但后来就测不到了。

此外像NRST一直为高,关键是TX-EN一直为低,同时,TX0、TX1都没有数据,这个我觉的就不对了,难道就是这个原因吗?帮我看看原理有没有问题?