This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

无法配置LMX2316

Other Parts Discussed in Thread: CODELOADER

       刚买到两块RF2915的开发板。上面的PLL芯片用的是LMX2316。我用信号发生器产生1MHz的正弦波,送入lmx2316的OSCin脚。安装了codeloader4,使用电脑并口配置。产生4MHz的频率。

      在codeloader里,选默认的LPT1口,选好器件,然后设定输入值和输出值。然后选择Load Device。但是芯片的fin脚并没有波形。FLo和CPo也没有波形,三个管脚都是低电平。

       测量Data脚:在Load Device时有5V脉冲出现。 后来我设置F[3]、F[4]、F[5],将FLo设置为Active High,测得的FLo还是低电平。

       将lmx2316的电源电压在3.6V和4.9V都试过,都无法配置。

希望专家能指点一下,多谢了!

  • 发现了一些错误:1、并口下载线缆是按照user guide做的,但是Codeloader里默认的点位跟user guide里的不一样,导致出现错误。重新定义了Codeloader里的点位,然后测量时序图,正确。并且将Fo/LD配置为Active High后,Fo/LD输出为高,正确。

    2、LMX2316的的fin为0.1~2.1GHz,最大fosc为5~40MHz。将信号发生器频率设为16MHz,由于示波器带宽仅为200MHz,所以输出频率设为一个较小的值,取120MHz。

    但是此时还有错误:

    一是此时fin、FLo和CPo仍没有波形。

    二是退出Codeloader后,Fo/LD的状态不能保持为高。感觉好像配置没有保存住。