This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC1101芯片的FIFOTHR寄存器

Other Parts Discussed in Thread: CC1101

在理解CC1101芯片的FIFOTHR寄存器上面感到比较困惑,手册中说A signal will assert when the number of bytes in the FIFO is equal to or higher than the programmed threshold. 在给的例子中说FIFO_THR=13,即在TX FIFO中的字节数equal to or higher than 9TX FIFO中字节数equal to or higher than 56时,会出现溢出。例子附的两个图也没明白:
   
需要请教的问题是:
1  FIFO_THR设置的是FIFO的最大值,为什么发送最大字节数是8,而接收能接收接收56字节?按照我的理解应该是最大发送8 byte,加上FEC2byte,接收端的门限应该是10byte才对,但从Figure 27中显示,为什么接收能有55byte,而发送只能有8 byte
2 我看SmartRF推荐配置为0x07,如果我想发送61字节,是否应该配置为0x00?