This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 关于High Speed Mode下参数的提问

Part Number: CC1310

我注意到其他模式(包括FSK、long range made、ook)下,在smartrf_settings_predefined.c中会配置deviation、symbolRate数值,具体结构体的声明如下:

struct {
      uint16_t modType:3;               //!< \brief 0: FSK<br>
                                        //!<        1: GFSK<br>
                                        //!<        Others: <i>Reserved</i>
      uint16_t deviation:13;            //!<        Deviation (250 Hz steps)
   } modulation;
   struct {
      uint32_t preScale:4;              //!<        Prescaler value
      uint32_t :4;
      uint32_t rateWord:21;             //!<        Rate word
      uint32_t decimMode:3;             //!< \brief 0: Use automatic PDIF decimation<br>
                                        //!<        1: Force PDIF decimation to 0<br>
                                        //!<        3: Force PDIF decimation to 1<br>
                                        //!<        5: Force PDIF decimation to 2<br>
                                        //!<        Others: <i>Reserved</i>
   } symbolRate;                        //!<        Symbol rate setting

但在smartrf_settings_predefined.c配置high speed mode时,我并没有找到这几个变量,具体配置如下:

rfc_CMD_RADIO_SETUP_t RF_cmdRadioSetup_hsm =
{
    .commandNo = CMD_RADIO_SETUP,
    .status = 0x0000,
    .pNextOp = 0x00000000,
    .startTime = 0x00000000,
    .startTrigger.triggerType = 0x0,
    .startTrigger.bEnaCmd = 0x0,
    .startTrigger.triggerNo = 0x0,
    .startTrigger.pastTrig = 0x0,
    .condition.rule = 0x1,
    .condition.nSkip = 0x0,
    .mode = 0x05,
    .loDivider = 5,
    .config.frontEndMode = 0x0,
    .config.biasMode = 0x1,
    .config.bNoFsPowerUp = 0,
    .txPower = 0x23F,
    .pRegOverride = pOverrides_hsm,
};

我该如何得到high speed mode下deviation、symbolRate的数值,或者可能的话,请告诉我这些数值。

P.S.使用的工程为rfPacketErrorRate

谢谢