您好:
现在我在使用CC1310 。电源1.9V 供电模式使用内部DCDC模式。目前测试拉高DIO5,发现DIO电平处于1.9V.在反复上电断点测试中。有概率会出现DIO电平只拉高到1.44V.查阅手册29页。发现手册说明在供电1.8V时。输出电压应该在1.54V左右。现在问题是,1:按照正常情况来说,IO口的输出电平应该和它的输入电平有关,这CC1310的DIO输出电平为什么比输入电平低0.3V左右。2:如果按照手册,输出电平为1.44V时为正常时,那为什么DIO会被拉高到1.9V?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
现在我在使用CC1310 。电源1.9V 供电模式使用内部DCDC模式。目前测试拉高DIO5,发现DIO电平处于1.9V.在反复上电断点测试中。有概率会出现DIO电平只拉高到1.44V.查阅手册29页。发现手册说明在供电1.8V时。输出电压应该在1.54V左右。现在问题是,1:按照正常情况来说,IO口的输出电平应该和它的输入电平有关,这CC1310的DIO输出电平为什么比输入电平低0.3V左右。2:如果按照手册,输出电平为1.44V时为正常时,那为什么DIO会被拉高到1.9V?