This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是由SmartRF Studio生成的寄存器配置。
// Address Config = No address check // Bit Rate = 1.2 // Carrier Frequency = 434.000000 // Deviation = 3.997803 // Device Address = 0 // Manchester Enable = false // Modulation Format = 2-FSK // PA Ramping = true // Packet Bit Length = 0 // Packet Length = 255 // Packet Length Mode = Variable // Performance Mode = High Performance // RX Filter BW = 10.000000 // Symbol rate = 1.2 // TX Power = 15 // Whitening = false #include "stdint.h" const uint16_t CC112X_REG_SETTING[][2]= { {0X0000,0X53},//IOCFG3 GPIO3 IO PIN CONFIGURATION {0X0001,0X46},//IOCFG2 GPIO2 IO PIN CONFIGURATION {0X0003,0X51},//IOCFG0 GPIO0 IO PIN CONFIGURATION {0X0008,0X0B},//SYNC_CFG1 SYNC WORD DETECTION CONFIGURATION REG. 1 {0X000C,0X1C},//DCFILT_CFG DIGITAL DC REMOVAL CONFIGURATION {0X0010,0XC6},//IQIC DIGITAL IMAGE CHANNEL COMPENSATION CONFIGURATION {0X0013,0X05},//MDMCFG0 GENERAL MODEM PARAMETER CONFIGURATION REG. 0 {0X0017,0X20},//AGC_REF AGC REFERENCE LEVEL CONFIGURATION {0X0018,0X19},//AGC_CS_THR CARRIER SENSE THRESHOLD CONFIGURATION {0X001C,0XA9},//AGC_CFG1 AUTOMATIC GAIN CONTROL CONFIGURATION REG. 1 {0X001D,0XCF},//AGC_CFG0 AUTOMATIC GAIN CONTROL CONFIGURATION REG. 0 {0X001E,0X00},//FIFO_CFG FIFO CONFIGURATION {0X0021,0X14},//FS_CFG FREQUENCY SYNTHESIZER CONFIGURATION {0X0028,0X20},//PKT_CFG0 PACKET CONFIGURATION REG. 0 {0X002E,0XFF},//PKT_LEN PACKET LENGTH CONFIGURATION {0X2F00,0X00},//IF_MIX_CFG IF MIX CONFIGURATION {0X2F01,0X22},//FREQOFF_CFG FREQUENCY OFFSET CORRECTION CONFIGURATION {0X2F0C,0X6C},//FREQ2 FREQUENCY CONFIGURATION [23:16] {0X2F0D,0X80},//FREQ1 FREQUENCY CONFIGURATION [15:8] {0X2F12,0X00},//FS_DIG1 FREQUENCY SYNTHESIZER DIGITAL REG. 1 {0X2F13,0X5F},//FS_DIG0 FREQUENCY SYNTHESIZER DIGITAL REG. 0 {0X2F16,0X40},//FS_CAL1 FREQUENCY SYNTHESIZER CALIBRATION REG. 1 {0X2F17,0X0E},//FS_CAL0 FREQUENCY SYNTHESIZER CALIBRATION REG. 0 {0X2F19,0X03},//FS_DIVTWO FREQUENCY SYNTHESIZER DIVIDE BY 2 {0X2F1B,0X33},//FS_DSM0 FS DIGITAL SYNTHESIZER MODULE CONFIGURATION REG. 0 {0X2F1D,0X17},//FS_DVC0 FREQUENCY SYNTHESIZER DIVIDER CHAIN CONFIGURATION .. {0X2F1F,0X50},//FS_PFD FREQUENCY SYNTHESIZER PHASE FREQUENCY DETECTOR CON.. {0X2F20,0X6E},//FS_PRE FREQUENCY SYNTHESIZER PRESCALER CONFIGURATION {0X2F21,0X14},//FS_REG_DIV_CML FREQUENCY SYNTHESIZER DIVIDER REGULATOR CONFIGURAT.. {0X2F22,0XAC},//FS_SPARE FREQUENCY SYNTHESIZER SPARE {0X2F27,0XB4},//FS_VCO0 FS VOLTAGE CONTROLLED OSCILLATOR CONFIGURATION REG.. {0X2F32,0X0E},//XOSC5 CRYSTAL OSCILLATOR CONFIGURATION REG. 5 {0X2F36,0X03},//XOSC1 CRYSTAL OSCILLATOR CONFIGURATION REG. 1 {0XFFFF,0XFF} };
经过我实际测试,当接上天线时,即使没有射频信号源存在,读取的RSSI值也高达-75dbm,一直在这个值左右波动。当我拔掉天线时,RSSI值就回落到-100dBm左右,很显然这个才是无信号时正常的值。RSSI值我已经用
软件进行了补偿,用仪器输入不同强度的射频信号,读取的RSSI值都是正常的,和仪器输出的强度误差在3dBm内。这应该说明RSSI指示寄存器是没有问题的。问题就在于:在没有射频信号时,为何读取的RSSI值会这么
高?请教一下这是什么原因引起的,要如何改善这个问题?这个问题对于接收性能影响太大了
补充说明一下:我已经尝试了在SmartRF Studio中使用不同的射频参数设置,并没有任何的变化或改善。
您好,我是自己做的板子。我也尝试通过用手去触摸板子上的元器件,希望能够看到RSSI数值能够改变,即使是更差。但是并没有任何的反应;我也对比了一下板子,没发现哪里有问题,板子的设计原理图我是照搬TI提供的参考设计,433段的。对于发射和接收灵敏度的测试,性能感觉还可以接受,发射的传导功率有14.5dBm,接收通过RSSI值来观察,可以做到-100dBm的灵敏度变化。当然肯定没有TI设计的开发板好,但是对于项目需求来说够用了。唯一的问题就是,当接上天线后,即使没有射频信号存在,RSSI值都比较高,大约在68--75dBm之间波动。拔掉天线后,数值就正常了。我用原来设计的CC1100E板子,读取RSSI对比,在相同频率下,CC1100E读取的RSSI值是没有 发现这个问题的。我不知道问题到底出在哪里,是因为CC1120接收灵敏度比CC1100E高吗?还是哪里设置错了?
对了,补充一下,当我输入更高的射频信号到CC1120,发现它的RSSI最高只能够显示-9dBm,就是说,高于这个强度的信号输入,RSSI被冻结在-9dBm了,不会变了。当信号降低后才恢复变化。这个是正常的吗?
非常感谢您的帮助,今天我调试了一天,反复把AGC相关的寄存器设置不同的值,唯一能够影响到RSSI值的只有AGC最大增益寄存器,当我把最大增益寄存器设置到和最小增益寄存器值时,反而RSSI值在无射频信号时比原来还增加了10dBm.除此以外,更改其他寄存器并没有发现有明显的变化。无论如何,当接上天线和拔掉天线,它们之间的RSSI值都会相差大约30dBm。我感觉这明显不对劲的,正常来说,在没有明显干扰的情况下,接上天线的RSSI增加不会超过10dBm才对,这还是基于高增益的接收机情况下。如果接收机增益低,这个差值应该会更低。可以麻烦你们那边用TI的开发板测试一下这个差异吗??就是接上天线和不接天线,RSSI差异是多少?? 我测试过非常多的频率,从450M-480M的频率区间我都测试过,470M以上的频率,差异会稍微低些,大约25dBm,而低于450M的就接近30dBm了。总体来说,都不太对劲
您好,请相信我做了非常多的基本测试,我肯定使用频谱分析仪测试过了环境噪声,但是除了看到手机信号塔的信号(868M,1.1G)和微弱的2.4G WIFI信号,并没有发现400M-500M这个频段有信号存在。另外,为了进一步确定并非是环境中其他信号造成的问题,我故意输入不同频段内的高强度信号到CC1120,发现CC1120的抗干扰能力非常强,RSSI值并没有因为有高强度的其他频段信号进入而出现明显的变化,这一点令我感到十分惊奇。为了证明那未知的信号来源是由天线接收到的,我用双手握住天线,发现RSSI值回落到-100dBm了,这令我更加确信,有我不知道的未知信号进入了CC1120。我尝试拿着板子到处走动,想尝试寻找信号源(如果靠近信号源,RSSI值应该会更强),但是失败了,没有找到能够让RSSI值更强的位置。但是经过测试判断信号又是从天线进入的,我是真的无奈了。我找不到也想不明白为什么,如果那个信号存在,为何找不到,看不到。如果不存在,为何RSSI会有这么高的强度指示
您好,我刚才直接用信号发生器输出了500M的+13dBm高强度射频信号给CC1120,CC1120工作在接收模式,频率为470M。发现了令我感到非常震惊的现象,之前一直没有尝试过这么靠近的频率测试,居然错过了这个现象。您猜怎么着?RSSI值居然降低了,它居然在接收了500M的+13dBm信号后,RSSI值降低到-103dBm了,这说明什么,说明了里面的AGC动作了,把前置增益降低了,而由于CC1120抗干扰太强,所以反而这时候RSSI值正常了。我想我找到真相了,真相就是CC1120真的接收到了未知信号,并且它承认了这个信号。
这是非常不合理的一点,真的。就算那个未知信号存在,但是它绝对是非法的。就像我的测试信号那样,它是非法的。但是由于CC1120内部前端增益太高,它把那个非法的信号放大了,这个是非常恐怖的一点。恐怖就恐怖在,CC1120在这时候没有了选频能力,它居然在这个时候失去了抗干扰这个功能。我想不明白,为什么??、基本可以确定,它是把噪声给放大了,所以才会出现不管任何频率,RSSI值都这么高,反而输入一个高强度的非法信号,RSSI值倒是变正常了,因为AGC动作了,前端增益降低了。我真的不知道如何是好了,它为什么要直接把非法信号放大,难道不应该先筛选频率吗??还是筛选失败了?由于噪声信号弱,筛选失败??请你们来帮助我,是不是能够通过寄存器什么设置来解决这个问题,我感觉这个问题不应该存在,这个问题是不合理的,正常来说,前端筛选信号,然后放大,不应该出现这种情况才对。是不是哪里设置得还不够好?
请相信我所有的寄存器设置都是用Smart RF studio生成的,我只是根据项目需求修改了部分设置,而我确信这部分设置不会造成这种影响。我重新上传这份设置麻烦你们帮忙看看
// Address Config = Address check, no broadcast // Bit Rate = 50 // Carrier Frequency = 434.000000 // Deviation = 24.963379 // Device Address = 0 // Manchester Enable = false // Modulation Format = 2-GFSK // PA Ramping = true // Packet Bit Length = 0 // Packet Length = 24 // Packet Length Mode = Variable // Performance Mode = High Performance // RX Filter BW = 100.000000 // Symbol rate = 50 // TX Power = 15 // Whitening = true #include "stdint.h" const uint16_t CC112X_REG_SETTING[][2]= { {0X0000,0X53},//IOCFG3 GPIO3 IO PIN CONFIGURATION {0X0001,0X46},//IOCFG2 GPIO2 IO PIN CONFIGURATION {0X0003,0X51},//IOCFG0 GPIO0 IO PIN CONFIGURATION {0X0008,0X08},//SYNC_CFG1 SYNC WORD DETECTION CONFIGURATION REG. 1 {0X000A,0X99},//DEVIATION_M FREQUENCY DEVIATION CONFIGURATION {0X000B,0X0D},//MODCFG_DEV_E MODULATION FORMAT AND FREQUENCY DEVIATION CONFIGUR.. {0X000C,0X15},//DCFILT_CFG DIGITAL DC REMOVAL CONFIGURATION {0X000D,0X18},//PREAMBLE_CFG1 PREAMBLE LENGTH CONFIGURATION REG. 1 {0X000F,0X3A},//FREQ_IF_CFG RX MIXER FREQUENCY CONFIGURATION {0X0010,0X00},//IQIC DIGITAL IMAGE CHANNEL COMPENSATION CONFIGURATION {0X0011,0X02},//CHAN_BW CHANNEL FILTER CONFIGURATION {0X0013,0X05},//MDMCFG0 GENERAL MODEM PARAMETER CONFIGURATION REG. 0 {0X0014,0X99},//SYMBOL_RATE2 SYMBOL RATE CONFIGURATION EXPONENT AND MANTISSA [1.. {0X0015,0X99},//SYMBOL_RATE1 SYMBOL RATE CONFIGURATION MANTISSA [15:8] {0X0016,0X99},//SYMBOL_RATE0 SYMBOL RATE CONFIGURATION MANTISSA [7:0] {0X0017,0X3C},//AGC_REF AGC REFERENCE LEVEL CONFIGURATION {0X0018,0XA1},//AGC_CS_THR CARRIER SENSE THRESHOLD CONFIGURATION {0X0019,0X9A},//AGC_GAIN_ADJUST RSSI OFFSET CONFIGURATION {0X001C,0XA9},//AGC_CFG1 AUTOMATIC GAIN CONTROL CONFIGURATION REG. 1 {0X001D,0XC0},//AGC_CFG0 AUTOMATIC GAIN CONTROL CONFIGURATION REG. 0 {0X0021,0X14},//FS_CFG FREQUENCY SYNTHESIZER CONFIGURATION {0X0026,0X00},//PKT_CFG2 PACKET CONFIGURATION REG. 2 {0X0027,0X55},//PKT_CFG1 PACKET CONFIGURATION REG. 1 {0X0028,0X20},//PKT_CFG0 PACKET CONFIGURATION REG. 0 {0X002D,0X79},//PA_CFG0 POWER AMPLIFIER CONFIGURATION REG. 0 {0X002E,0X18},//PKT_LEN PACKET LENGTH CONFIGURATION {0X2F00,0X00},//IF_MIX_CFG IF MIX CONFIGURATION {0X2F02,0X0A},//TOC_CFG TIMING OFFSET CORRECTION CONFIGURATION {0X2F0C,0X6C},//FREQ2 FREQUENCY CONFIGURATION [23:16] {0X2F0D,0X80},//FREQ1 FREQUENCY CONFIGURATION [15:8] {0X2F12,0X00},//FS_DIG1 FREQUENCY SYNTHESIZER DIGITAL REG. 1 {0X2F13,0X5F},//FS_DIG0 FREQUENCY SYNTHESIZER DIGITAL REG. 0 {0X2F16,0X40},//FS_CAL1 FREQUENCY SYNTHESIZER CALIBRATION REG. 1 {0X2F17,0X0E},//FS_CAL0 FREQUENCY SYNTHESIZER CALIBRATION REG. 0 {0X2F19,0X03},//FS_DIVTWO FREQUENCY SYNTHESIZER DIVIDE BY 2 {0X2F1B,0X33},//FS_DSM0 FS DIGITAL SYNTHESIZER MODULE CONFIGURATION REG. 0 {0X2F1D,0X17},//FS_DVC0 FREQUENCY SYNTHESIZER DIVIDER CHAIN CONFIGURATION .. {0X2F1F,0X50},//FS_PFD FREQUENCY SYNTHESIZER PHASE FREQUENCY DETECTOR CON.. {0X2F20,0X6E},//FS_PRE FREQUENCY SYNTHESIZER PRESCALER CONFIGURATION {0X2F21,0X14},//FS_REG_DIV_CML FREQUENCY SYNTHESIZER DIVIDER REGULATOR CONFIGURAT.. {0X2F22,0XAC},//FS_SPARE FREQUENCY SYNTHESIZER SPARE {0X2F27,0XB4},//FS_VCO0 FS VOLTAGE CONTROLLED OSCILLATOR CONFIGURATION REG.. {0X2F32,0X0E},//XOSC5 CRYSTAL OSCILLATOR CONFIGURATION REG. 5 {0X2F36,0X03},//XOSC1 CRYSTAL OSCILLATOR CONFIGURATION REG. 1 {0XFFFF,0XFF} };
您好,
1. CC1120 EVM在同样环境下表现如何?
2. 传导测试RSSI结果如何?
3. 改变环境(例如到空旷室外)对结果有何影响?
Best regards,
Shuyang
您好,EVM我没有进行过测试,传导测试的RSSI基本是正常的,我从-90dBm到0dBm这个范围内测试过传导接收灵敏度,RSSI指示误差在5dBm以内,主要表现是弱信号RSSI指示很精准,就是强信号时大约会有4dBm的误差,当信号超过-5dBm时,RSSI冻结在-9dBm不再变化。这个可以接受。发射传导功率会死14.5dBm。我也在不同的环境测试过,例如地下车库,电梯里面,室内。由于我在城市地区,没有在绝对空旷的环境进行过测试。在不同环境下,RSSI表现有相当明显的变化,例如在电梯内,RSSI会比其他地方低大约10dB左右。我也测试过将天线摆放在不同的角度,有个别的角度RSSI会低至-100dBm,显然这个是正常的。我现在非常怀疑是手机发射塔的信号噪声对CC1120造成了干扰,因为不管我在哪里,接上天线后CC1120的RSSI值都无法保持低于-100dBm,只能在个别角度下会达成。
传导测试正常说明芯片接收机是正常的,至于环境中有噪声的时候CC1120前端增益是否有改变,这个需要咨询产品线了。建议您到英文E2E论坛上问一下(e2e.ti.com),上面会有产品线的工程师来回答。
如果要自己验证的话,还是建议找个EVM进行一下对比,如果EVM没问题而您的板子有问题的话,再考虑修改硬件设计。
Best regards,
Shuyang
哎,今天我找了个带外衰减为-40dB的介质滤波器装上去测试,有改善,但是无法完全解决问题,无信号时RSSI依然还在-90dBm左右波动,比原来好些。我想买个你们TI那个开发板回来测试一下是否也是如此,因为实在我看不出我自己的板子哪里有问题。不知TI那个CC1120的开发板,要在哪里买呢?可以提供一下链接吗,谢谢
CC1120EMK-420-470:
https://www.ti.com/tool/CC1120EMK-420-470
搭配SMARTRFTRXEBK:
https://www.ti.com/tool/SMARTRFTRXEBK
可以评估433MHz频段。
Best regards,
Shuyang