Part Number: CC1310
Other Parts Discussed in Thread: SYSCONFIG,
我在使用CC1310RGZ芯片时,使用了PIN的中断,然后在回调函数内使用SPI的DMA功能。在调试的时候进入SPI通信失败了,程序卡死了。在中断外部能却够使用该SPI通信。这是优先级的原因导致的吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
能将您的工程文件打包发过来测试一下吗?这将对我们确定问题很有帮助。
另外,您说您使用了Sysconfig配置了文件?CC1310并不支持Sysconfig,您这是怎么操作的?
您好,我这边用的离线端的SYSCONFIG,通过浏览本地的SDK路径进入配置的。CC1310这边的外围电路是我自己画的,并没有使用CC1310_LaunchPad;工程文件里的三个文件CC1310_LAUNCHXL.c CC1310_LAUNCHXL.h CC1310_LAUNCHXL_fxns.c我删除了,使用的配置文件Board.c和Board,h。
/*
* ======== Board.c ========
* Configured TI-Drivers module definitions
*
* DO NOT EDIT - This file is generated for the CC1310RGZ
* by the SysConfig tool.
*/
#include <stddef.h>
#ifndef DeviceFamily_CC13X0
#define DeviceFamily_CC13X0
#endif
#include <ti/devices/DeviceFamily.h>
#include "Board.h"
/*
* =============================== DMA ===============================
*/
#include <ti/drivers/dma/UDMACC26XX.h>
#include <ti/devices/cc13x0/driverlib/udma.h>
#include <ti/devices/cc13x0/inc/hw_memmap.h>
UDMACC26XX_Object udmaCC26XXObject;
const UDMACC26XX_HWAttrs udmaCC26XXHWAttrs = {
.baseAddr = UDMA0_BASE,
.powerMngrId = PowerCC26XX_PERIPH_UDMA,
.intNum = INT_DMA_ERR,
.intPriority = 0xC0
};
const UDMACC26XX_Config UDMACC26XX_config[1] = {
{
.object = &udmaCC26XXObject,
.hwAttrs = &udmaCC26XXHWAttrs,
},
};
/*
* =============================== GPIO ===============================
*/
#include <ti/drivers/GPIO.h>
#include <ti/drivers/gpio/GPIOCC26XX.h>
/*
* ======== gpioPinConfigs ========
* Array of Pin configurations
*/
GPIO_PinConfig gpioPinConfigs[] = {
/* SPI_SS */
GPIOCC26XX_DIO_21 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_HIGH,
/* INT1 */
GPIOCC26XX_DIO_14 | GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_NONE,
};
/*
* ======== GPIOCC26XX_config ========
*/
const GPIOCC26XX_Config GPIOCC26XX_config = {
.pinConfigs = (GPIO_PinConfig *)gpioPinConfigs,
.callbacks = NULL,
.numberOfPinConfigs = 2,
.numberOfCallbacks = 0,
.intPriority = (~0)
};
/*
* =============================== PIN ===============================
*/
#include <ti/drivers/PIN.h>
#include <ti/drivers/pin/PINCC26XX.h>
const PIN_Config BoardGpioInitTable[] = {
/* Parent Signal: ADXL372 SCLK, (DIO22) */
Board_PIN0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MED,
/* Parent Signal: ADXL372 MISO, (DIO18) */
Board_PIN1 | PIN_INPUT_EN | PIN_NOPULL | PIN_IRQ_DIS,
/* Parent Signal: ADXL372 MOSI, (DIO19) */
Board_PIN2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MED,
/* Parent Signal: SPI_SS GPIO Pin, (DIO21) */
Board_PIN3 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH | PIN_PUSHPULL | PIN_DRVSTR_MED,
/* Parent Signal: INT1 GPIO Pin, (DIO14) */
Board_PIN4 | PIN_INPUT_EN | PIN_PULLUP | PIN_IRQ_DIS,
/* Parent Signal: UART0 TX, (DIO3) */
Board_PIN5 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MED,
/* Parent Signal: UART0 RX, (DIO2) */
Board_PIN6 | PIN_INPUT_EN | PIN_PULLDOWN | PIN_IRQ_DIS,
PIN_TERMINATE
};
const PINCC26XX_HWAttrs PINCC26XX_hwAttrs = {
.intPriority = (~0),
.swiPriority = 0
};
/*
* =============================== Power ===============================
*/
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
#include "Board.h"
extern void PowerCC26XX_standbyPolicy(void);
extern bool PowerCC26XX_calibrate(unsigned int);
const PowerCC26XX_Config PowerCC26XX_config = {
.enablePolicy = true,
.policyInitFxn = NULL,
.policyFxn = PowerCC26XX_standbyPolicy,
.calibrateFxn = PowerCC26XX_calibrate,
.vddrRechargeMargin = 0,
.calibrateRCOSC_LF = true,
.calibrateRCOSC_HF = true,
};
/*
* =============================== SPI DMA ===============================
*/
#include <ti/drivers/SPI.h>
#include <ti/drivers/spi/SPICC26XXDMA.h>
#define Board_SPICOUNT 1
/*
* ======== spiCC26XXDMAObjects ========
*/
SPICC26XXDMA_Object spiCC26XXDMAObjects[Board_SPICOUNT];
/*
* ======== spiCC26XXDMAHWAttrs ========
*/
const SPICC26XXDMA_HWAttrsV1 spiCC26XXDMAHWAttrs[Board_SPICOUNT] = {
/* ADXL372 */
{
.baseAddr = SSI0_BASE,
.intNum = INT_SSI0_COMB,
.intPriority = 0xc0,
.swiPriority = 1,
.powerMngrId = PowerCC26XX_PERIPH_SSI0,
.defaultTxBufValue = ~0,
.rxChannelBitMask = 1<<UDMA_CHAN_SSI0_RX,
.txChannelBitMask = 1<<UDMA_CHAN_SSI0_TX,
.minDmaTransferSize = 10,
.mosiPin = IOID_19,
.misoPin = IOID_18,
.clkPin = IOID_22,
.csnPin = PIN_UNASSIGNED
},
};
/*
* ======== SPI_config ========
*/
const SPI_Config SPI_config[Board_SPICOUNT] = {
/* ADXL372 */
{
.fxnTablePtr = &SPICC26XXDMA_fxnTable,
.object = &spiCC26XXDMAObjects[ADXL372],
.hwAttrs = &spiCC26XXDMAHWAttrs[ADXL372]
},
};
const uint_least8_t SPI_count = Board_SPICOUNT;
/*
* =============================== UART ===============================
*/
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/UARTCC26XX.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
#include <ti/devices/cc13x0/inc/hw_memmap.h>
#include <ti/devices/cc13x0/inc/hw_ints.h>
#define Board_UARTCOUNT 1
UARTCC26XX_Object uartCC26XXObjects[Board_UARTCOUNT];
static unsigned char uartCC26XXRingBuffer0[32];
static const UARTCC26XX_HWAttrsV2 uartCC26XXHWAttrs[Board_UARTCOUNT] = {
{
.baseAddr = UART0_BASE,
.intNum = INT_UART0_COMB,
.intPriority = (~0),
.swiPriority = 0,
.powerMngrId = PowerCC26XX_PERIPH_UART0,
.ringBufPtr = uartCC26XXRingBuffer0,
.ringBufSize = sizeof(uartCC26XXRingBuffer0),
.rxPin = IOID_2,
.txPin = IOID_3,
.ctsPin = PIN_UNASSIGNED,
.rtsPin = PIN_UNASSIGNED,
.txIntFifoThr = UARTCC26XX_FIFO_THRESHOLD_1_8,
.rxIntFifoThr = UARTCC26XX_FIFO_THRESHOLD_4_8,
.errorFxn = NULL
},
};
const UART_Config UART_config[Board_UARTCOUNT] = {
{ /* UART0 */
.fxnTablePtr = &UARTCC26XX_fxnTable,
.object = &uartCC26XXObjects[0],
.hwAttrs = &uartCC26XXHWAttrs[0]
},
};
const uint_least8_t UART_count = Board_UARTCOUNT;
#include <ti/drivers/Board.h>
/*
* ======== Board_initHook ========
* Perform any board-specific initialization needed at startup. This
* function is declared weak to allow applications to override it if needed.
*/
#if defined(__IAR_SYSTEMS_ICC__)
__weak void Board_initHook(void)
#elif defined(__GNUC__) && !defined(__ti__)
void __attribute__((weak)) Board_initHook(void)
#else
#pragma WEAK (Board_initHook)
void Board_initHook(void)
#endif
{
}
/*
* ======== Board_init ========
* Perform any initialization needed before using any board APIs
*/
void Board_init(void)
{
/* ==== /ti/drivers/Power initialization ==== */
Power_init();
/* ==== /ti/drivers/PIN initialization ==== */
if (PIN_init(BoardGpioInitTable) != PIN_SUCCESS) {
/* Error with PIN_init */
while (1);
}
Board_initHook();
}
/*
* ======== Board.h ========
* Configured TI-Drivers module declarations
*
* DO NOT EDIT - This file is generated for the CC1310RGZ
* by the SysConfig tool.
*/
#ifndef Board_h
#define Board_h
#define Board_SYSCONFIG_PREVIEW
#define Board_CC1310RGZ
/* Temporary define for backwards compatibility!!! */
#define __CC1310RGZ_BOARD_H__
#ifndef DeviceFamily_CC13X0
#define DeviceFamily_CC13X0
#endif
#include <stdint.h>
/* support C++ sources */
#ifdef __cplusplus
extern "C" {
#endif
/*
* ======== GPIO ========
*/
#define SPI_SS 0
#define INT1 1
/* LEDs are active high */
#define Board_GPIO_LED_ON (1)
#define Board_GPIO_LED_OFF (0)
#define Board_LED_ON (Board_GPIO_LED_ON)
#define Board_LED_OFF (Board_GPIO_LED_OFF)
/*
* ======== PIN ========
*/
/* Includes */
#include <ti/drivers/PIN.h>
/* Externs */
extern const PIN_Config BoardGpioInitTable[];
/* Parent Signal: ADXL372 SCLK, (DIO22) */
#define Board_PIN0 0x00000016
/* Parent Signal: ADXL372 MISO, (DIO18) */
#define Board_PIN1 0x00000012
/* Parent Signal: ADXL372 MOSI, (DIO19) */
#define Board_PIN2 0x00000013
/* Parent Signal: SPI_SS GPIO Pin, (DIO21) */
#define Board_PIN3 0x00000015
/* Parent Signal: INT1 GPIO Pin, (DIO14) */
#define Board_PIN4 0x0000000e
/* Parent Signal: UART0 TX, (DIO3) */
#define Board_PIN5 0x00000003
/* Parent Signal: UART0 RX, (DIO2) */
#define Board_PIN6 0x00000002
/*
* ======== SPI ========
*/
#define ADXL372 0
/*
* ======== UART ========
*/
#define UART0 0
/*
* ======== Board_init ========
* Perform all required TI-Drivers initialization
*
* This function should be called once at a point before any use of
* TI-Drivers.
*/
extern void Board_init(void);
/*
* ======== Board_initGeneral ========
* (deprecated)
*
* Board_initGeneral() is defined purely for backward compatibility.
*
* All new code should use Board_init() to do any required TI-Drivers
* initialization _and_ use <Driver>_init() for only where specific drivers
* are explicitly referenced by the application. <Driver>_init() functions
* are idempotent.
*/
#define Board_initGeneral Board_init
#ifdef __cplusplus
}
#endif
#endif /* include guard */
您好,
由于CC1310的SDK本身不支持SYSCONFIG,所以您这么导入有可能会造成不可预期的错误。(相关寄存器配置问题之类的)
您这边为什么需要使用sysconfig?CC1310的话还是建议直接修改文件如图:
。
您好,
是的,您需要修改相关文件的包括 CC1310_LAUNCHXL.c CC1310_LAUNCHXL.h Board,h 的代码(如上一条回复的图所示)。