This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 关于在433M应用时,数据率和 SPI通信速度问题

Part Number: CC1310
Other Parts Discussed in Thread: CC1350

1、在433M应用时,相关软件是否可以支持4Mbps的数据率?

2、目前应用想通过CC1310的SPI接口做为从设备,由其他芯片给cc1310传输数据,速度大约4Mbps。然后再由射频用4Mbps传输,是否可以实现上述应用? 如果spi无法实现上述应用,是否有其他方案可以?

3、对于上述的应用,如果CC1310无法实现,是否由其他芯片可以? 我们的需求是低功耗的433M无线射频芯片,可以不含mcu,数据率大于4Mbps,可以通过高速SPI等接口与其他MCU传输数据.thx