Other Parts Discussed in Thread: CC1310
你好,我像请问一下官方文档timer.h里面的ui32Base赋值应该怎么赋值,见附图,这具体是一个什么地址,感谢解答。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我像请问一下官方文档timer.h里面的ui32Base赋值应该怎么赋值,见附图,这具体是一个什么地址,感谢解答。

CC1310的两个延时函数:CPUdelay(8000*50);和Task_sleep(1000);
Task_sleep会放弃执行本任务,转去执行其他任务;CPUdelay只是延迟执行时间。一般来说两个都能用
CPUdelay使用delay loop来实现延时,其延时单位为指令周期。
//*****************************************************************************
//
//! \brief Provide a small delay.
//!
//! This function provides means for generating a constant length delay. It
//! is written in assembly to keep the delay consistent across tool chains,
//! avoiding the need to tune the delay based on the tool chain in use.
//!
//! The loop takes 3 cycles/loop.
//!
//! \param ui32Count is the number of delay loop iterations to perform.
//!
//! \return None
//
//*****************************************************************************
extern void CPUdelay(uint32_t ui32Count);
Task_sleep是让出对MCU的占用,可以让其他task得到执行或者执行idle task从而进入低功耗状态。它的计时单位是systick,默认为10us。