This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,使用2.4G的无线射频芯片,如何增加发送距离,有没有专用的增益芯片?
谢谢
2.4G是个标准的频点,市场上有很多射频放大器的厂商。你也可以看看固定121,15,18dB增益的TRF37A75,B75和C75
上面回答有一处笔误,是12dB,不是121dB
谢谢您!
TI的目前供2.4GHz 私有协议芯片用的PA+LNA射频前端主推 CC2592。