This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

谁做过 cc2530芯片 外接 RF1100SE 做无线通讯

Other Parts Discussed in Thread: CC2530, CC1100

球分享下思路      弄了一天没头绪啊

  • 请问能否详细描述下你的问题? 

  • 可以  就是我用cc2530   外接RFCC1100SE 无线模块 做无线遥控学习,

    根据1100文档    需要用cc2530的spi给1100写配置    我根据51单片机的demo 更改  代码如下

    #include <ioCC2530.h>
    //#include <intrins.h>
    #define INT8U unsigned char
    #define INT16U unsigned int

    #define WRITE_BURST 0x40 //连续写入
    #define READ_SINGLE 0x80 //读
    #define READ_BURST 0xC0 //连续读
    #define BYTES_IN_RXFIFO 0x7F //接收缓冲区的有效字节数
    #define CRC_OK 0x80 //CRC校验通过位标志
    //***********************************CC1100接口*************************************************
    //sbit GDO0 =P3^3;
    //sbit GDO2 =P1^4;
    //sbit MISO =P1^2;
    //sbit MOSI =P1^1;
    //sbit SCK =P3^2;
    //sbit CSN =P1^3;

    #define MISO P1_7
    #define MOSI P1_6
    #define SCK P1_5
    #define GDO0 P1_4
    //#define GDO2 P1_3
    #define CSN P1_2
    //***********************************按键********************************************************
    //sbit KEY1 =P3^6;
    //sbit KEY2 =P3^7;
    #define KEY1 P0_4
    #define KEY2 P0_5
    //***********************************数码管位选**************************************************
    //sbit led3=P2^0;
    //sbit led2=P2^1;
    //sbit led1=P2^2;
    //sbit led0=P2^3;
    #define LED1 P1_0
    #define LED2 P1_1
    //***********************************蜂鸣器*******************************************************
    //sbit BELL=P3^4;
    //***************更多功率参数设置可详细参考DATACC1100英文文档中第48-49页的参数表******************
    //INT8U PaTabel[8] = {0x04 ,0x04 ,0x04 ,0x04 ,0x04 ,0x04 ,0x04 ,0x04}; //-30dBm 功率最小
    INT8U PaTabel[8] = {0x60 ,0x60 ,0x60 ,0x60 ,0x60 ,0x60 ,0x60 ,0x60}; //0dBm
    //INT8U PaTabel[8] = {0xC0 ,0xC0 ,0xC0 ,0xC0 ,0xC0 ,0xC0 ,0xC0 ,0xC0}; //10dBm 功率最大
    //***********************************************************************************************
    void SpiInit(void);
    void CpuInit(void);
    void RESET_CC1100(void);
    void POWER_UP_RESET_CC1100(void);
    void halSpiWriteReg(INT8U addr, INT8U value);
    void halSpiWriteBurstReg(INT8U addr, INT8U *buffer, INT8U count);
    void halSpiStrobe(INT8U strobe);
    INT8U halSpiReadReg(INT8U addr);
    void halSpiReadBurstReg(INT8U addr, INT8U *buffer, INT8U count);
    INT8U halSpiReadStatus(INT8U addr);
    void halRfWriteRfSettings(void);
    void halRfSendPacket(INT8U *txBuffer, INT8U size);
    INT8U halRfReceivePacket(INT8U *rxBuffer, INT8U *length);
    //*****************************************************************************************
    // CC1100 STROBE, CONTROL AND STATUS REGSITER
    #define CC2530_IOCFG2 0x00 // GDO2 output pin configuration
    #define CC2530_IOCFG1 0x01 // GDO1 output pin configuration
    #define CC2530_IOCFG0 0x02 // GDO0 output pin configuration
    #define CC2530_FIFOTHR 0x03 // RX FIFO and TX FIFO thresholds
    #define CC2530_SYNC1 0x04 // Sync word, high INT8U
    #define CC2530_SYNC0 0x05 // Sync word, low INT8U
    #define CC2530_PKTLEN 0x06 // Packet length
    #define CC2530_PKTCTRL1 0x07 // Packet automation control
    #define CC2530_PKTCTRL0 0x08 // Packet automation control
    #define CC2530_ADDR 0x09 // Device address
    #define CC2530_CHANNR 0x0A // Channel number
    #define CC2530_FSCTRL1 0x0B // Frequency synthesizer control
    #define CC2530_FSCTRL0 0x0C // Frequency synthesizer control
    #define CC2530_FREQ2 0x0D // Frequency control word, high INT8U
    #define CC2530_FREQ1 0x0E // Frequency control word, middle INT8U
    #define CC2530_FREQ0 0x0F // Frequency control word, low INT8U
    #define CC2530_MDMCFG4 0x10 // Modem configuration
    #define CC2530_MDMCFG3 0x11 // Modem configuration
    #define CC2530_MDMCFG2 0x12 // Modem configuration
    #define CC2530_MDMCFG1 0x13 // Modem configuration
    #define CC2530_MDMCFG0 0x14 // Modem configuration
    #define CC2530_DEVIATN 0x15 // Modem deviation setting
    #define CC2530_MCSM2 0x16 // Main Radio Control State Machine configuration
    #define CC2530_MCSM1 0x17 // Main Radio Control State Machine configuration
    #define CC2530_MCSM0 0x18 // Main Radio Control State Machine configuration
    #define CC2530_FOCCFG 0x19 // Frequency Offset Compensation configuration
    #define CC2530_BSCFG 0x1A // Bit Synchronization configuration
    #define CC2530_AGCCTRLI2 0x1B // AGC control
    #define CC2530_AGCCTRLI1 0x1C // AGC control
    #define CC2530_AGCCTRLI0 0x1D // AGC control
    #define CC2530_WOREVT1 0x1E // High INT8U Event 0 timeout
    #define CC2530_WOREVT0 0x1F // Low INT8U Event 0 timeout
    #define CC2530_WORCTRL 0x20 // Wake On Radio control
    #define CC2530_FREND1 0x21 // Front end RX configuration
    #define CC2530_FREND0 0x22 // Front end TX configuration
    #define CC2530_FSCALI3 0x23 // Frequency synthesizer calibration
    #define CC2530_FSCALI2 0x24 // Frequency synthesizer calibration
    #define CC2530_FSCALI1 0x25 // Frequency synthesizer calibration
    #define CC2530_FSCALI0 0x26 // Frequency synthesizer calibration
    #define CC2530_RCCTRL1 0x27 // RC oscillator configuration
    #define CC2530_RCCTRL0 0x28 // RC oscillator configuration
    #define CC2530_FSTEST 0x29 // Frequency synthesizer calibration control
    #define CC2530_PTEST 0x2A // Production test
    #define CC2530_AGCTEST 0x2B // AGC test
    #define CC2530_TEST2 0x2C // Various test settings
    #define CC2530_TEST1 0x2D // Various test settings
    #define CC2530_TEST0 0x2E // Various test settings

    // Strobe commands
    #define CC2530_SRES 0x30 // Reset chip.
    #define CC2530_SFSTXON 0x31 // Enable and calibrate frequency synthesizer (if MCSM0.FS_AUTOCAL=1).
    // If in RX/TX: Go to a wait state where only the synthesizer is
    // running (for quick RX / TX turnaround).
    #define CC2530_SXOFF 0x32 // Turn off crystal oscillator.
    #define CC2530_SCAL 0x33 // Calibrate frequency synthesizer and turn it off
    // (enables quick start).
    #define CC2530_SRX 0x34 // Enable RX. Perform calibration first if coming from IDLE and
    // MCSM0.FS_AUTOCAL=1.
    #define CC2530_STX 0x35 // In IDLE state: Enable TX. Perform calibration first if
    // MCSM0.FS_AUTOCAL=1. If in RX state and CCA is enabled:
    // Only go to TX if channel is clear.
    #define CC2530_SIDLE 0x36 // Exit RX / TX, turn off frequency synthesizer and exit
    // Wake-On-Radio mode if applicable.
    #define CC2530_SAFC 0x37 // Perform AFC adjustment of the frequency synthesizer
    #define CC2530_SWOR 0x38 // Start automatic RX polling sequence (Wake-on-Radio)
    #define CC2530_SPWD 0x39 // Enter power down mode when CSn goes high.
    #define CC2530_SFRX 0x3A // Flush the RX FIFO buffer.
    #define CC2530_SFTX 0x3B // Flush the TX FIFO buffer.
    #define CC2530_SWORRST 0x3C // Reset real time clock.
    #define CC2530_SNOP 0x3D // No operation. May be used to pad strobe commands to two
    // INT8Us for simpler software.

    #define CC2530_PARTNUM 0x30
    #define CC2530_VERSION 0x31
    #define CC2530_FREQEST 0x32
    #define CC2530_LQI 0x33
    #define CC2530_RSSI 0x34
    #define CC2530_MARCSTATE 0x35
    #define CC2530_WORTIME1 0x36
    #define CC2530_WORTIME0 0x37
    #define CC2530_PKTSTATUS 0x38
    #define CC2530_VCO_VC_DAC 0x39
    #define CC2530_TXBYTES 0x3A
    #define CC2530_RXBYTES 0x3B

    #define CC2530_PATABLE 0x3E
    #define CC2530_TXFIFO 0x3F
    #define CC2530_RXFIFO 0x3F

    // RF_SETTINGS is a data structure which contains all relevant CC2530 registers
    typedef struct S_RF_SETTINGS
    {
    INT8U FSCTRL2; //自已加的
    INT8U FSCTRL1; // Frequency synthesizer control.
    INT8U FSCTRL0; // Frequency synthesizer control.
    INT8U FREQ2; // Frequency control word, high INT8U.
    INT8U FREQ1; // Frequency control word, middle INT8U.
    INT8U FREQ0; // Frequency control word, low INT8U.
    INT8U MDMCFG4; // Modem configuration.
    INT8U MDMCFG3; // Modem configuration.
    INT8U MDMCFG2; // Modem configuration.
    INT8U MDMCFG1; // Modem configuration.
    INT8U MDMCFG0; // Modem configuration.
    INT8U CHANNR; // Channel number.
    INT8U DEVIATN; // Modem deviation setting (when FSK modulation is enabled).
    INT8U FREND1; // Front end RX configuration.
    INT8U FREND0; // Front end RX configuration.
    INT8U MCSM0; // Main Radio Control State Machine configuration.
    INT8U FOCCFG; // Frequency Offset Compensation Configuration.
    INT8U BSCFG; // Bit synchronization Configuration.
    INT8U AGCCTRLI2; // AGC control.
    INT8U AGCCTRLI1; // AGC control.
    INT8U AGCCTRLI0; // AGC control.
    INT8U FSCALI3; // Frequency synthesizer calibration.
    INT8U FSCALI2; // Frequency synthesizer calibration.
    INT8U FSCALI1; // Frequency synthesizer calibration.
    INT8U FSCALI0; // Frequency synthesizer calibration.
    INT8U FSTEST; // Frequency synthesizer calibration control
    INT8U TEST2; // Various test settings.
    INT8U TEST1; // Various test settings.
    INT8U TEST0; // Various test settings.
    INT8U IOCFG2; // GDO2 output pin configuration
    INT8U IOCFG0; // GDO0 output pin configuration
    INT8U PKTCTRL1; // Packet automation control.
    INT8U PKTCTRL0; // Packet automation control.
    INT8U ADDR; // Device address.
    INT8U PKTLEN; // Packet length.
    } RF_SETTINGS;

    /////////////////////////////////////////////////////////////////
    const RF_SETTINGS rfSettings =
    {
    0x00,
    0x08, // FSCTRL1 Frequency synthesizer control.
    0x00, // FSCTRL0 Frequency synthesizer control.
    0x10, // FREQ2 Frequency control word, high byte.
    0xA7, // FREQ1 Frequency control word, middle byte.
    0x62, // FREQ0 Frequency control word, low byte.
    0x5B, // MDMCFG4 Modem configuration.
    0xF8, // MDMCFG3 Modem configuration.
    0x03, // MDMCFG2 Modem configuration.
    0x22, // MDMCFG1 Modem configuration.
    0xF8, // MDMCFG0 Modem configuration.

    0x00, // CHANNR Channel number.
    0x47, // DEVIATN Modem deviation setting (when FSK modulation is enabled).
    0xB6, // FREND1 Front end RX configuration.
    0x10, // FREND0 Front end RX configuration.
    0x18, // MCSM0 Main Radio Control State Machine configuration.
    0x1D, // FOCCFG Frequency Offset Compensation Configuration.
    0x1C, // BSCFG Bit synchronization Configuration.
    0xC7, // AGCCTRL2 AGC control.
    0x00, // AGCCTRL1 AGC control.
    0xB2, // AGCCTRL0 AGC control.

    0xEA, // FSCAL3 Frequency synthesizer calibration.
    0x2A, // FSCAL2 Frequency synthesizer calibration.
    0x00, // FSCAL1 Frequency synthesizer calibration.
    0x11, // FSCAL0 Frequency synthesizer calibration.
    0x59, // FSTEST Frequency synthesizer calibration.
    0x81, // TEST2 Various test settings.
    0x35, // TEST1 Various test settings.
    0x09, // TEST0 Various test settings.
    0x0B, // IOCFG2 GDO2 output pin configuration.
    0x06, // IOCFG0D GDO0 output pin configuration. Refer to SmartRF?Studio User Manual for detailed pseudo register explanation.

    0x04, // PKTCTRL1 Packet automation control.
    0x05, // PKTCTRL0 Packet automation control.
    0x00, // ADDR Device address.
    0x0c // PKTLEN Packet length.
    };
    //*****************************************************************************************
    //函数名:delay(unsigned int s)
    //输入:时间
    //输出:无
    //功能描述:普通廷时,内部用
    //*****************************************************************************************
    static void delay(unsigned int s)
    {
    unsigned int i;
    for(i=0; i<s; i++);
    for(i=0; i<s; i++);
    }


    void halWait(INT16U timeout)
    {
    do
    {
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    asm("NOP");
    } while (--timeout);
    }


    void SpiInit(void)
    {
    CSN=0;
    SCK=0;
    CSN=1;
    //MISO=0;
    }

    /*****************************************************************************************
    //函数名:CpuInit()
    //输入:无
    //输出:无
    //功能描述:SPI初始化程序
    /*****************************************************************************************/
    void CpuInit(void)
    {
    SpiInit();
    delay(5000);
    }

    //*****************************************************************************************
    //函数名:SpisendByte(INT8U dat)
    //输入:发送的数据
    //输出:无
    //功能描述:SPI发送一个字节
    //*****************************************************************************************
    INT8U SpiTxRxByte(INT8U dat)
    {
    INT8U i,temp;
    temp = 0;

    SCK = 0;
    for(i=0; i<8; i++)
    {
    if(dat & 0x80)
    {
    MOSI = 1;
    }
    else
    {
    MOSI = 0;
    }
    dat <<= 1;

    SCK = 1;
    asm("NOP");
    asm("NOP");

    temp <<= 1;
    if(MISO)temp++;
    SCK = 0;
    asm("NOP");
    asm("NOP");
    }
    return temp;
    }

    //*****************************************************************************************
    //函数名:void RESET_CC1100(void)
    //输入:无
    //输出:无
    //功能描述:复位CC1100
    //*****************************************************************************************
    void RESET_CC1100(void)
    {
    CSN = 0;
    while (MISO);
    SpiTxRxByte(CC2530_SRES); //写入复位命令
    while (MISO);
    CSN = 1;
    }

    //*****************************************************************************************
    //函数名:void POWER_UP_RESET_CC1100(void)
    //输入:无
    //输出:无
    //功能描述:上电复位CC1100
    //*****************************************************************************************
    void POWER_UP_RESET_CC1100(void)
    {
    CSN = 1;
    halWait(1);
    CSN = 0;
    halWait(1);
    CSN = 1;
    halWait(41);
    RESET_CC1100(); //复位CC1100
    }

    //*****************************************************************************************
    //函数名:void halSpiWriteReg(INT8U addr, INT8U value)
    //输入:地址和配置字
    //输出:无
    //功能描述:SPI写寄存器
    //*****************************************************************************************
    void halSpiWriteReg(INT8U addr, INT8U value)
    {
    CSN = 0;
    while (MISO);
    SpiTxRxByte(addr); //写地址
    SpiTxRxByte(value); //写入配置
    CSN = 1;
    }

    //*****************************************************************************************
    //函数名:void halSpiWriteBurstReg(INT8U addr, INT8U *buffer, INT8U count)
    //输入:地址,写入缓冲区,写入个数
    //输出:无
    //功能描述:SPI连续写配置寄存器
    //*****************************************************************************************
    void halSpiWriteBurstReg(INT8U addr, INT8U *buffer, INT8U count)
    {
    INT8U i, temp;
    temp = addr | WRITE_BURST;
    CSN = 0;
    while (MISO);
    SpiTxRxByte(temp);
    for (i = 0; i < count; i++)
    {
    SpiTxRxByte(buffer[i]);
    }
    CSN = 1;
    }

    //*****************************************************************************************
    //函数名:void halSpiStrobe(INT8U strobe)
    //输入:命令
    //输出:无
    //功能描述:SPI写命令
    //*****************************************************************************************
    void halSpiStrobe(INT8U strobe)
    {
    CSN = 0;
    while (MISO);
    SpiTxRxByte(strobe); //写入命令
    CSN = 1;
    }

    //*****************************************************************************************
    //函数名:INT8U halSpiReadReg(INT8U addr)
    //输入:地址
    //输出:该寄存器的配置字
    //功能描述:SPI读寄存器
    //*****************************************************************************************
    INT8U halSpiReadReg(INT8U addr)
    {
    INT8U temp, value;
    temp = addr|READ_SINGLE;//读寄存器命令
    CSN = 0;
    while (MISO);
    SpiTxRxByte(temp);
    value = SpiTxRxByte(0);
    CSN = 1;
    return value;
    }


    //*****************************************************************************************
    //函数名:void halSpiReadBurstReg(INT8U addr, INT8U *buffer, INT8U count)
    //输入:地址,读出数据后暂存的缓冲区,读出配置个数
    //输出:无
    //功能描述:SPI连续写配置寄存器
    //*****************************************************************************************
    void halSpiReadBurstReg(INT8U addr, INT8U *buffer, INT8U count)
    {
    INT8U i,temp;
    temp = addr | READ_BURST; //写入要读的配置寄存器地址和读命令
    CSN = 0;
    while (MISO);
    SpiTxRxByte(temp);
    for (i = 0; i < count; i++)
    {
    buffer[i] = SpiTxRxByte(0);
    }
    CSN = 1;
    }


    //*****************************************************************************************
    //函数名:INT8U halSpiReadReg(INT8U addr)
    //输入:地址
    //输出:该状态寄存器当前值
    //功能描述:SPI读状态寄存器
    //*****************************************************************************************
    INT8U halSpiReadStatus(INT8U addr)
    {
    INT8U value,temp;
    temp = addr | READ_BURST; //写入要读的状态寄存器的地址同时写入读命令
    CSN = 0;
    while (MISO);
    SpiTxRxByte(temp);
    value = SpiTxRxByte(0);
    CSN = 1;
    return value;
    }
    //*****************************************************************************************
    //函数名:void halRfWriteRfSettings(RF_SETTINGS *pRfSettings)
    //输入:无
    //输出:无
    //功能描述:配置CC1100的寄存器
    //*****************************************************************************************
    void halRfWriteRfSettings(void)
    {

    halSpiWriteReg(CC2530_FSCTRL0, rfSettings.FSCTRL2);//自已加的
    // Write register settings
    halSpiWriteReg(CC2530_FSCTRL1, rfSettings.FSCTRL1);
    halSpiWriteReg(CC2530_FSCTRL0, rfSettings.FSCTRL0);
    halSpiWriteReg(CC2530_FREQ2, rfSettings.FREQ2);
    halSpiWriteReg(CC2530_FREQ1, rfSettings.FREQ1);
    halSpiWriteReg(CC2530_FREQ0, rfSettings.FREQ0);
    halSpiWriteReg(CC2530_MDMCFG4, rfSettings.MDMCFG4);
    halSpiWriteReg(CC2530_MDMCFG3, rfSettings.MDMCFG3);
    halSpiWriteReg(CC2530_MDMCFG2, rfSettings.MDMCFG2);
    halSpiWriteReg(CC2530_MDMCFG1, rfSettings.MDMCFG1);
    halSpiWriteReg(CC2530_MDMCFG0, rfSettings.MDMCFG0);
    halSpiWriteReg(CC2530_CHANNR, rfSettings.CHANNR);
    halSpiWriteReg(CC2530_DEVIATN, rfSettings.DEVIATN);
    halSpiWriteReg(CC2530_FREND1, rfSettings.FREND1);
    halSpiWriteReg(CC2530_FREND0, rfSettings.FREND0);
    halSpiWriteReg(CC2530_MCSM0 , rfSettings.MCSM0 );
    halSpiWriteReg(CC2530_FOCCFG, rfSettings.FOCCFG);
    halSpiWriteReg(CC2530_BSCFG, rfSettings.BSCFG);
    halSpiWriteReg(CC2530_AGCCTRLI2, rfSettings.AGCCTRLI2);
    halSpiWriteReg(CC2530_AGCCTRLI1, rfSettings.AGCCTRLI1);
    halSpiWriteReg(CC2530_AGCCTRLI0, rfSettings.AGCCTRLI0);
    halSpiWriteReg(CC2530_FSCALI3, rfSettings.FSCALI3);
    halSpiWriteReg(CC2530_FSCALI2, rfSettings.FSCALI2);
    halSpiWriteReg(CC2530_FSCALI1, rfSettings.FSCALI1);
    halSpiWriteReg(CC2530_FSCALI0, rfSettings.FSCALI0);
    halSpiWriteReg(CC2530_FSTEST, rfSettings.FSTEST);
    halSpiWriteReg(CC2530_TEST2, rfSettings.TEST2);
    halSpiWriteReg(CC2530_TEST1, rfSettings.TEST1);
    halSpiWriteReg(CC2530_TEST0, rfSettings.TEST0);
    halSpiWriteReg(CC2530_IOCFG2, rfSettings.IOCFG2);
    halSpiWriteReg(CC2530_IOCFG0, rfSettings.IOCFG0);
    halSpiWriteReg(CC2530_PKTCTRL1, rfSettings.PKTCTRL1);
    halSpiWriteReg(CC2530_PKTCTRL0, rfSettings.PKTCTRL0);
    halSpiWriteReg(CC2530_ADDR, rfSettings.ADDR);
    halSpiWriteReg(CC2530_PKTLEN, rfSettings.PKTLEN);
    }

    //*****************************************************************************************
    //函数名:void halRfSendPacket(INT8U *txBuffer, INT8U size)
    //输入:发送的缓冲区,发送数据个数
    //输出:无
    //功能描述:CC1100发送一组数据
    //*****************************************************************************************

    void halRfSendPacket(INT8U *txBuffer, INT8U size)
    {
    halSpiWriteReg(CC2530_TXFIFO, size);
    halSpiWriteBurstReg(CC2530_TXFIFO, txBuffer, size); //写入要发送的数据

    halSpiStrobe(CC2530_STX); //进入发送模式发送数据

    // Wait for GDO0 to be set -> sync transmitted
    while (!GDO0);
    // Wait for GDO0 to be cleared -> end of packet
    while (GDO0);
    halSpiStrobe(CC2530_SFTX);
    }


    void setRxMode(void)
    {
    halSpiStrobe(CC2530_SRX); //进入接收状态
    }

    /*
    // Bit masks corresponding to STATE[2:0] in the status byte returned on MISO
    #define CCxx00_STATE_BM 0x70
    #define CCxx00_FIFO_BYTES_AVAILABLE_BM 0x0F
    #define CCxx00_STATE_TX_BM 0x20
    #define CCxx00_STATE_TX_UNDERFLOW_BM 0x70
    #define CCxx00_STATE_RX_BM 0x10
    #define CCxx00_STATE_RX_OVERFLOW_BM 0x60
    #define CCxx00_STATE_IDLE_BM 0x00

    static INT8U RfGetRxStatus(void)
    {
    INT8U temp, spiRxStatus1,spiRxStatus2;
    INT8U i=4;// 循环测试次数
    temp = CC2530_SNOP|READ_SINGLE;//读寄存器命令
    CSN = 0;
    while (MISO);
    SpiTxRxByte(temp);
    spiRxStatus1 = SpiTxRxByte(0);
    do
    {
    SpiTxRxByte(temp);
    spiRxStatus2 = SpiTxRxByte(0);
    if(spiRxStatus1 == spiRxStatus2)
    {
    if( (spiRxStatus1 & CCxx00_STATE_BM) == CCxx00_STATE_RX_OVERFLOW_BM)
    {
    halSpiStrobe(CC2530_SFRX);
    return 0;
    }
    return 1;
    }
    spiRxStatus1=spiRxStatus2;
    }
    while(i--);
    CSN = 1;
    return 0;
    }
    */
    INT8U halRfReceivePacket(INT8U *rxBuffer, INT8U *length)
    {
    INT8U status[2];
    INT8U packetLength;
    INT8U i=(*length)*4; // 具体多少要根据datarate和length来决定

    halSpiStrobe(CC2530_SRX); //进入接收状态
    //delay(5);
    //while (!GDO1);
    //while (GDO1);
    delay(2);
    while(GDO0)
    {
    delay(2);
    --i;
    if(i<1)
    return 0;
    }
    if ((halSpiReadStatus(CC2530_RXBYTES) & BYTES_IN_RXFIFO)) //如果接的字节数不为0
    {
    packetLength = halSpiReadReg(CC2530_RXFIFO);//读出第一个字节,此字节为该帧数据长度
    if (packetLength <= *length) //如果所要的有效数据长度小于等于接收到的数据包的长度
    {
    halSpiReadBurstReg(CC2530_RXFIFO, rxBuffer, packetLength); //读出所有接收到的数据
    *length = packetLength; //把接收数据长度的修改为当前数据的长度

    // Read the 2 appended status bytes (status[0] = RSSI, status[1] = LQI)
    halSpiReadBurstReg(CC2530_RXFIFO, status, 2); //读出CRC校验位
    halSpiStrobe(CC2530_SFRX); //清洗接收缓冲区
    return (status[1] & CRC_OK); //如果校验成功返回接收成功
    }
    else
    {
    *length = packetLength;
    halSpiStrobe(CC2530_SFRX); //清洗接收缓冲区
    return 0;
    }
    }
    else
    {
    return 0;
    }
    }

    /*
    void Delay(unsigned int s)
    {
    unsigned int i;
    for(i=0; i<s; i++);
    for(i=0; i<s; i++);
    }

    */
    void main(void)
    {

    INT8U leng =0;
    INT8U tf =0;
    INT8U TxBuf[8]={0}; // 8字节, 如果需要更长的数据包,请正确设置
    INT8U RxBuf[8]={0};
    P1DIR |= 0x03;
    //BELL=0;
    CpuInit();
    POWER_UP_RESET_CC1100();
    halRfWriteRfSettings();
    halSpiWriteBurstReg(CC2530_PATABLE, PaTabel, 8);

    //TxBuf[0] = 8 ;
    //TxBuf[1] = 1 ;
    //TxBuf[2] = 1 ;
    //halRfSendPacket(TxBuf,8); // Transmit Tx buffer data
    delay(6000);
    P0=0xBF;
    //led0=0;led1=0;led2=0;led3=0;
    LED1=0;LED2=0;
    //BELL=1;
    while(1)
    {
    //setRxMode();
    if(KEY1 ==0 )
    {
    TxBuf[1] = 1;
    TxBuf[2] = 0;
    tf = 1 ;
    delay(500);
    LED1 = 1;
    //while(KEY1 ==0);
    }
    if(KEY2 ==0 )
    {
    TxBuf[1] = 0;
    TxBuf[2] = 1;
    tf = 1 ;
    delay(500);
    LED2 = 1;
    }
    if(tf==1)
    {
    halRfSendPacket(TxBuf,8); // Transmit Tx buffer data
    //TxBuf[1] = 0xff;
    //TxBuf[2] = 0xff;
    tf=0;
    delay(500);
    //led0=0;led1=0;led2=0;led3=0;
    //LED1=1;LED2=1;
    }

    leng =8; // 预计接受8 bytes
    if(halRfReceivePacket(RxBuf,&leng))
    {

    if(RxBuf[1]==1)
    {
    P0=0xF7;
    //led0=0;led1=0;led2=0;led3=0;
    LED1=0;LED2=0;
    }
    if(RxBuf[2]==1)
    {
    P0=0xFE;
    //led0=0;led1=0;led2=0;led3=0;
    }
    delay(1000);
    LED1=1;LED2=1;
    //led0=1;led1=1;led2=1;led3=1;
    }
    //LED1=1;LED2=1;
    RxBuf[1] = 0xff;
    RxBuf[2] = 0xff;
    }
    }

    问题是  接收不到无线遥控器发来的数据!!!