This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: 使用CC1312R官方开发板和例程配合使用,出现CCS工程编译不通过

Part Number: CC1312R

T"syscfg/ti_drivers_config.o" -I"C:/Users/Administrator/workspace_v13/rfPacketTx_CC1312R1_LAUNCHXL_tirtos7_ticlang/Debug/syscfg" -o"syscfg/ti_drivers_config.o" "syscfg/ti_drivers_config.c"
subdir_rules.mk:34: recipe for target 'syscfg/ti_drivers_config.o' failed
In file included from syscfg/ti_drivers_config.c:124:
In file included from C:/ti/simplelink_cc13xx_cc26xx_sdk_7_10_01_24/source\ti/drivers/rf/RF.h:54:
C:/ti/simplelink_cc13xx_cc26xx_sdk_7_10_01_24/source\ti/drivers/rf/RFCC26X2.h:2237:12: error: expected ')'
(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent);
^
C:/ti/simplelink_cc13xx_cc26xx_sdk_7_10_01_24/source\ti/drivers/rf/RFCC26X2.h:2237:1: note: to match this '('
(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent);
^
C:/ti/simplelink_cc13xx_cc26xx_sdk_7_10_01_24/source\ti/drivers/rf/RFCC26X2.h:2237:2: error: redefinition of 'RF_Handle' as different kind of symbol
(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent);
^
C:/ti/simplelink_cc13xx_cc26xx_sdk_7_10_01_24/source\ti/drivers/rf/RFCC26X2.h:1505:20: note: previous definition is here
typedef RF_Object* RF_Handle;
^
2 errors generated.
gmake: *** [syscfg/ti_drivers_config.o] Error 1
gmake: Target 'all' not remade because of errors.