This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: CC1312 rfpacketRx例程信号强度rssi是如何读取的

Part Number: CC1312R


只有easylink例程里面有信号强度rssi数据么?

  • 在rfPacketRx例程中有相关代码,

    具体分为两种方式

    方式一:在接收数据包时读取RSSI值  使用bAppendRsii

    方式二:读取当前信道的信号强度,使用RF_getRssi()

    可以参考以下帖子

    https://e2echina.ti.com/support/wireless-connectivity/sub-1-ghz/f/sub-1-ghz-forum/146298/cc1310-rssi/458210#458210

  • RF_getRssi()

    这条命令读出来的是0x80是错误的。

    bAppendRsii

    能否具体说明一下呢?没看明白

  • 使用bAppendRssi是在每次收到的数据包后面附上接收时的RSSI数值,注意设置接收缓存时,留出足够空间存放RSSI值。

    /* Packet RX Configuration */
    #define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */
    #define MAX_LENGTH 30 /* Max length byte the radio will accept */
    #define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */
    #define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain:
                                                                  * 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
                                                                  * Max 30 payload bytes
                                                                  * 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */

    rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
                                                                                                          MAX_LENGTH,
                                                                                                          NUM_APPENDED_BYTES)];

  • RF_getRssi()使用时需要射频处于接收状态

    void *mainThread(void *arg0)
    {
    RF_Params rfParams;
    RF_Params_init(&rfParams);

    /* Request access to the radio */
    rfHandle = RF_open(&rfObject, &RF_prop,
    (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
    /*设置为连续接收模式*/
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdRxTest, RF_PriorityNormal, NULL, 0);
    while(1)
    {
    temp=RF_getRssi(rfHandle);
    };
    }