Part Number: CC1311R3
Other Parts Discussed in Thread: CC1310
如题,我们有一个项目需要比CC1310的端口多和SRAM比较大,我们选择了CC1311R3。我们以前CC1310 HS模式通讯速度在433MHZ能达到1.5M,CC1311R3有没有这个高速模式?或者有没有计划退出像CC1310那样的高速补丁?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC1311 的最高 characterized 数据速率为 1 Mbps。
我们用smartRF Studio做了一些测试,在修改一些设置后最高能够以1.5 Mbps的速度接收数据包。由于我们无法保证此数据速率下的性能(灵敏度、选择性、阻塞等),这没有被披露出来。 无法实现HS模式
1.最高表征数据速率可达1Mbps
2.关于补丁目前是没有确切消息的