Part Number: CC1312R
您好
我看到CC1312R使用了M4F的内核,资料中提到其具有FPU和MPU,但未提到DSP。
而CC1314使用了M33内核,资料中提到有MPU、DSP,没有提到有FPU。
请问这两个芯片这部分设计不同吗?或者对于数字信号处理的能力究竟是否一致?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
CC1312R和CC1314使用的内核不同,但它们都支持数字信号处理。
CC1312R采用的是Cortex-M4F内核,其内置了一个浮点运算单元(FPU),该FPU可在硬件层面上对浮点运算进行加速。同时,它还支持DSP指令集,这使得它可以高效地执行数字信号处理操作。
而CC1314采用的是Cortex-M33内核,它内置了一个数字信号处理器(DSP),可以高效地执行数字信号处理操作。但是,与CC1312R不同的是,Cortex-M33内核没有内置FPU,因此在执行浮点运算时需要通过软件模拟来实现。
总之,虽然CC1312R和CC1314使用了不同的内核,但它们都可以支持数字信号处理功能。CC1312R通过内置的FPU和支持DSP指令集来提供数字信号处理能力,而CC1314则通过内置的DSP来提供数字信号处理能力。