This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: RTC CH0和CH1 的compare事件是否有冲突

Part Number: CC1310

请问CC1310的RTC CH0和CH1的compare定时器事件是否存在冲突,如下是我的在CC1310_LAUNCHXL开发板上跑的测试代码,我用了RTC CH1的compare定时器,已经实现了红灯一秒闪烁,但是发现绿灯没有1秒闪烁,程序好像一直卡在INT_AON_RTC_COMB的中断回调函数里面出不来,这是什么原因呢?是程序正常运行的时候开了RTC CH0的compare,所以我现在用RTC CH1的compare,影响到程序正常运行了吗?

//rtc channel1 compare事件中断回调函数
void rtc_ch1_interrupt_handler(void)
{
  //清除事件标志
  AONRTCEventClear(AON_RTC_CH1);
  IntPendClear(INT_AON_RTC_COMB);
  //开发板绿灯引脚电平转换
  GPIO_toggleDio(IOID_6);
  //重新生成1秒事件
  AONRTCCompareValueSet(AON_RTC_CH1, (AONRTCCurrentCompareValueGet() + FACTOR_SEC_TO_COMP_VAL_FORMAT));
}

void rtc_ch1_compare_timer_init(void)
{
  AONRTCChannelEnable(AON_RTC_CH1); //启用通道1
  AONRTCModeCh1Set(AON_RTC_MODE_CH1_COMPARE); //启用CH1捕获模式
  AONRTCCompareValueSet(AON_RTC_CH1, FACTOR_SEC_TO_COMP_VAL_FORMAT); // 1秒后生成事件
  AONRTCCombinedEventConfig(AON_RTC_CH1);
  IntRegister(INT_AON_RTC_COMB, rtc_ch1_interrupt_handler);
  IntEnable(INT_AON_RTC_COMB); //开启compare事件中断
}

int main(void)
{
  //CC1310 Nortos启动
  Power_init();
  PIN_init(BoardGpioInitTable);
  NoRTOS_start();

  //开发板红灯引脚初始化为输出低
  GPIO_setOutputEnableDio(IOID_6, GPIO_OUTPUT_ENABLE);
  GPIO_writeDio(IOID_6, PIN_LOW);

  //开发板绿灯引脚初始化为输出低
  GPIO_setOutputEnableDio(IOID_7, GPIO_OUTPUT_ENABLE);
  GPIO_writeDio(IOID_7, PIN_LOW);

  //初始化RTC channel 1 compare事件
  rtc_ch1_compare_timer_init();

  while(1)
  {
    //绿灯间隔一秒闪烁
    GPIO_toggleDio(IOID_7);
    sleep(1);
  }
}