This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC115L: cc115L与cc1101通信

Part Number: CC115L
Other Parts Discussed in Thread: CC1101, , CC110L

大家好!

我们正在进行cc115L和cc1101的通信对接,我们使用Setup_SmartRF_Studio_7-2.30.0配置了相同的expert mode,选择的Generic 868MHz的第四个,也就是Data rate:2.4kBaud,Dev:5.2kHz,Mod:GFSK,RX BW:58KHz,Optimized for sensitvity。

我们将cc115L作为TX,cc1101作为RX。微型控制器里完全按照Register View配置了cc115L,其中作为RX的cc1101我们还和TX的cc1101验证过,能正常通讯,但是用cc115L去发消息,cc1101并没有收到,从cc115L打印的数据来看,长度和数据都写进了TX FIFO,并且使能TX后,也处于发射模式,但是cc1101一直没有收到数据,没有反应。

调试情况如下;

(1)在软件上:为了确定cc115L寄存器配置和TXFIFO是否配置正确,我们还将数据读出检查,没有问题。

(2)硬件上:有现成的cc115lL作为TX与cc110L作为RX能正常通信,说明硬件没问题。

我想请教,我需要你们帮助我查看数据怎么修改,或者一些调试的建议

配置如下图: