This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R7: OAD程序MCU_BOOT的引导地址设置

Part Number: CC1312R7


Hi,Team Ti:

关于CC1312R7的OAD功能,目前应用程序我使用的例程是:ns_coap_oad_offchip_src_LP_CC1312R7_tirtos7_ticlang(版本:simplelink_cc13xx_cc26xx_sdk_7_10_01_24),BOOT代码使用的是:mcuboot_LP_CC1312R7_nortos_ticlang,现在我需要扩大MCU_BOOT的空间(16KB 扩大为24KB),我尝试在mcuboot_cc13x2x7_cc26x2x7.cmd中修改了FLASH_BASE为0xAA000,FLASH_SIZE修改为0x6000;然后在C:\ti\simplelink_cc13xx_cc26xx_sdk_7_10_01_24\source\third_party\mcuboot\boot\ti\source\mcuboot_app\flash_map_backend\flash_map_backend.h 文件中修改BOOTLOADER_BASE_ADDRESS 为0x000AA000,BOOT_BOOTLOADER_SIZE 修改为0x00005FA8,然后重新编译该工程,同时下载到开发板中,但重启开发板并没有执行BOOT程序,请问还需要设置哪里吗?