Part Number: CC1310
Hi team, I am using the CC1310 RTOS this code is in a while(1),I found that it's consuming time is about 180ms(approxiately),is the consuming time in this while(1) correct 50kbps rfpacketTX?and then I noticed that the current also seems to be relatively high than CC1310 datasheet explained.
/* 待机定时10秒 */
sleepTickCount = 1000000 / Clock_tickPeriod;
//UART_write(uart,&by, 1);
while(1){
ledPinHandle = PIN_open(&ledPinState, pinTable);
// IOCPinTypeGpioOutput(0x1);
ADC_init();
ADC_Handle adc;
ADC_Params params;
int_fast16_t res;
ADC_Params_init(¶ms);
adc = ADC_open(CC1310_LAUNCHXL_ADC7 , ¶ms);
if (adc == NULL)
{
while (1);
}
/* Blocking mode conversion */
res = ADC_convert(adc, &adcValue0);
packet[4]=adcValue0 & 0xFF;
packet[5]=adcValue0;
if (res == ADC_STATUS_SUCCESS) {
adcValue0MicroVolt = ADC_convertRawToMicroVolts(adc, adcValue0);
packet[0] =(adcValue0MicroVolt >> 24) & 0xFF; // 获取高8位
packet[1] =(adcValue0MicroVolt >> 16) & 0xFF; // 获取次高8位
packet[2]= (adcValue0MicroVolt >> 8) & 0xFF; // 获取次低8位
packet[3] = adcValue0MicroVolt & 0xFF;
// UART_write(uart,&byte, 4);
double X= (double)adcValue0MicroVolt; // 将 adcValue0MicroVolt 转换为 double 类型的变量 number
uint16_t integer_part;
calculate_R(X, &integer_part);
double ln_R = log(integer_part); // 计算ln(R)
double result=3950/(ln_R+4.038);
result= result-273.15;
uint8_t xx=(uint8_t)result;//取整
double erWithTwoDecimals = result * 100; // 将原始数乘以 100,以保留两位小数
uint16_t xy = (uint16_t)erWithTwoDecimals;
uint8_t de = xy % 100;
packet[4]=xx;
packet[5]=de;
packet[6]=1;
// sprintf("%d",packet[6]);
packet[7]=1;
//UART_write(uart,&packet, 8);
// sprintf(byte[0],"%d",30);
// UART_write(uart,&byte, 1);
// sprintf(ascii_array[0],"%d",packet[6]);
// UART_write(uart,&ascii_array, 1);
}
// Task_sleep(sleepTickCount);
ADC_close(adc);
PIN_close(ledPinHandle);
ledPinHandle = PIN_open(&ledPinState, shutTable);
// PIN_setOutputValue(ledPinHandle, CC1310_LAUNCHXL_PIN_RLED , !PIN_getOutputValue(CC1310_LAUNCHXL_PIN_RLED ));
// usleep(10000);
// PIN_setOutputValue(ledPinHandle, CC1310_LAUNCHXL_PIN_RLED , !PIN_getOutputValue(CC1310_LAUNCHXL_PIN_RLED ));
// UART_write(uart, &input, 2);
// AONBatMonDisable ();
/* Request access to the radio */
#if defined(DeviceFamily_CC26X0R2)
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioSetup, &rfParams);
#else
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
#endif// DeviceFamily_CC26X0R2
// RF_cmdPropRadioDivSetup.txPower=0x913F;
//设置频率
RF_CmdHandle txTestHnle=RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
/* Create packet with incrementing sequence number and random payload */
// packet[0] = input[0];
uint8_t i;
for (i = 7; i < PAYLOAD_LENGTH; i++)
{
packet[i] = 1;
}
xor_encrypt_decrypt(packet, key, PAYLOAD_LENGTH);
/* Send packet */
RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropTx,
RF_PriorityNormal, NULL, 0);//stuck on this step
// switch(terminationReason)
// {
// case RF_EventLastCmdDone:
// // A stand-alone radio operation command or the last radio
// // operation command in a chain finished.
// break;
// case RF_EventCmdCancelled:
// // Command cancelled before it was started; it can be caused
// // by RF_cancelCmd() or RF_flushCmd().
// break;
// case RF_EventCmdAborted:
// // Abrupt command termination caused by RF_cancelCmd() or
// // RF_flushCmd().
// break;
// case RF_EventCmdStopped:
// // Graceful command termination caused by RF_cancelCmd() or
// // RF_flushCmd().
// break;
// default:
// // Uncaught error event
// while(1);
// }
//
// uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropTx)->status;
// switch(cmdStatus)
// {
// case PROP_DONE_OK:
// // 传输包成功
// break;
// case PROP_DONE_STOPPED:
// // received CMD_STOP while transmitting packet and finished
// // transmitting packet
// break;
// case PROP_DONE_ABORT:
// // Received CMD_ABORT while transmitting packet
// break;
// case PROP_ERROR_PAR:
// // Observed illegal parameter
// break;
// case PROP_ERROR_NO_SETUP:
// // Command sent without setting up the radio in a supported
// // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP
// break;
// case PROP_ERROR_NO_FS:
// // Command sent without the synthesizer being programmed
// break;
// case PROP_ERROR_TXUNF:
// // TX underflow observed during operation
// break;
// default:
// // Uncaught error event - these could come from the
// // pool of states defined in rf_mailbox.h
// while(1);
// }
#ifndef POWER_MEASUREMENT
// PIN_setOutputValue(ledPinHandle, Board_PIN_LED1,!PIN_getOutputValue(Board_PIN_LED1));
#endif
/* Power down the radio */
RF_yield(rfHandle);
#ifdef POWER_MEASUREMENT
/* Sleep for PACKET_INTERVAL s */
sleep(PACKET_INTERVAL);
#else
/* Sleep for PACKET_INTERVAL us */
usleep(PACKET_INTERVAL);
#endif
RF_cancelCmd(rfHandle,txTestHnle,0);
// RF_flushCmd (rfHandle,txTestHnle,1); //擦除
RF_yield(rfHandle); //断电
RF_close(rfHandle);
PIN_close(ledPinHandle);
Task_sleep(sleepTickCount);
}