This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 外部晶振和通信问题

Expert 2290 points

Part Number: CC1310

CC1310 两块板, 一块使用48M外部晶振, 一块使用24M晶振,   

1. 48M的板子和24M的板子不能通信, 接收不到数据

2. 48M的板子和 LAUNCHXL-CC1310 也无法通信

3. 24M的板子和 LAUNCHXL-CC1310 可以通信

请问不同频率的外部晶振导致无法通信是什么原因?

  • 您好

    https://www.ti.com/lit/ds/symlink/cc1310.pdf

    根据datasheet以下原文说明外部时钟使用24MHz

    The CC1310 device supports two external and two internal clock sources. A 24-MHz external crystal is required as the frequency reference for the radio. This signal is doubled internally to create a 48-MHz clock. The 32.768-kHz crystal is optional. The low-speed crystal oscillator is designed for use with a 32.768-kHz watch-type crystal. The internal high-speed RC oscillator (48-MHz) can be used as a clock source for the CPU subsystem. The internal low-speed RC oscillator (32-kHz) can be used as a reference if the low-power crystal oscillator is not used. The 32-kHz clock source can be used as external clocking reference through GPIO。

    请您参考(datasheet的第42页Clock Systems部分)

  • 外部晶振只能使用24M的吗?

  • 您好

    感谢您的回复!
    根据datasheet推荐是24MHz。详细说明如上回复的说明。