如题:技术支持说CC2538不宜与CC2530混用,请问具体原因是什么呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
理论上是可以共用的。可以参考 http://e2e.ti.com/support/wireless_connectivity/f/158/p/334938/1169311
您现在的应用环境是怎样的?
CC2530作为协调器,CC2538作为终端。因为原产品是以CC2530开发的。新产品中2530的资源不足,换用CC2538作为终端。因在小批量中出现一些问题,在询问技术支持时,说是不宜用CC2530做协调器。
另请问我们在生产中发现,CC2530的32M晶振频率偏低,CC2538的偏高。个别会出因为频偏原因不能正常通信,表现为:协调器可以收到终端的请求,协调器也下发了允许,但终端不能入网。在调整晶振频偏后,该现象排除。想了解一下,TI官方是否有批量生产时,晶振的调试指导说明。我看手册中有介绍微调功能。那有没有比较详细的指导。
再有。我们在CC2538SF23时,晶振不起振。我们的软件工程师说是STACK是基于SF53的。对SF23不支持。请问是怎么回事。谢谢!
你好 Susan Yang,我现在需要用cc2538做协调器,cc2530作为终端和路由,
请问我需要用哪个版本的协议栈,用什么开发环境呢???
原来我用的都是cc2530,协议栈用的是ZStack-CC2530-2.3.0-1.4.0协议栈,开发工具用的是IAR EW8051 V8.1,仿真器用的是SmartRF04EB仿真器驱动.rar。
谢谢!!!
开发环境的话,您需要使用IAR,建议使用新版本。
协议栈的话,您可以根据您的具体应用环境进行选择 http://www.ti.com.cn/tool/cn/z-stack
ZSTACK-HOME是可以支持CC2530和CC2538的
您好,我跟您遇到同样的问题,请问这个问题后来怎么解决的?要换协议栈吗?换协议栈后能和ZStack-CC2530-2.3.0-1.4.0协议栈设备通信吗?
您好,yunayin shi ,我现在一个毕业设计是用CC2538做一个协调器,希望能跟您交流一下,能帮我一下。
23的要用如下的icf文件:
//*****************************************************************************
//
// Linker configuration file for CC2538.
//
// Copyright (c) 2012-2013 Texas Instruments Incorporated. All rights reserved.
//
//*****************************************************************************
//
// Define a memory region that covers the entire 4 GB addressible space of the
// processor.
//
define memory mem with size = 4G;
//
// Define a region for the on-chip program code space.
//
define region FLASH = mem:[from 0x00200000 to 0x0023C7FF];
//
// Define a region for the OTA CRC structure.
//
//define region CRC = mem:[from 0x002001EC to 0x002001F3];
//
// Define a region for the OTA Preamble structure.
//
//define region PREAMBLE = mem:[from 0x002001F4 to 0x002001FF];
//
// Define a region for the NVIC table that is 512-byte aligned.
//
//define region INTVEC = mem:[from 0x00200200 to 0x002003FF];
//
// Define a region for the on-chip non-volatile (NV) memory.
// "HAL_NV_PAGE_CNT" pages of on-chip flash memory (originally 6 pages) are
// designated for Z-Stack NV items to be stored outside program code space.
// The size of this region MUST MATCH the size defined by "HAL_NV_PAGE_CNT"
// in the file: hal_board_cfg.h
//
define region NV_MEM = mem:[from 0x0023C800 to 0x0023F7FF];
//
// Define regions for on-chip factory Commissioning Parameters.
// One page of on-chip flash memory (originally page 255) is designated
// for various parameters to be "commissioned" outside program code space.
//
// Key-Establishment "Implicit Certificate"
define region CP_IMPC = mem:[from 0x0023FF6C to 0x0023FF9B];
//
// Key-Establishment "Certificate Authority Public Key"
define region CP_CAPK = mem:[from 0x0023FF9C to 0x0023FFB3];
//
// Key-Establishment "Device Private Key"
define region CP_DEPK = mem:[from 0x0023FFB4 to 0x0023FFCB];
//
// Device's unique 64-bit IEEE address
define region CP_IEEE = mem:[from 0x0023FFCC to 0x0023FFD3];
//
// Define a region for Customer Configuration Area in flash.
define region FLASH_CCA = mem:[from 0x0023FFD4 to 0x0023FFDF];
//
// Define the region for Lock Bits in flash.
define region FLASH_LCK = mem:[from 0x0023FFE0 to 0x0023FFFF];
//
// Define the region for Image Boot Manager (IBM) Ledger Page.
//define region LEDGER_PAGE = mem:[from 0x0023C000 to 0x0023C7FF];
//
// Define the region for Image Boot Manager (IBM)
//define region BOOTLOADER_PAGE = mem:[from 0x0023F800 to 0x0023FD00];
//
// Define a region for the on-chip SRAM.
//
define region SRAM = mem:[from 0x20004000 to 0x20007FFF];
//
// Define a block for the heap. The size should be set to something other
// than zero if things in the C library that require the heap are used.
//
define block HEAP with alignment = 8, size = 0x00000100 { };
//
// Indicate that the read/write values should be initialized by copying from
// flash.
//
initialize by copy { readwrite };
//
// Indicate that the noinit values should be left alone. This includes the
// stack, which if initialized will destroy the return address from the
// initialization code, causing the processor to branch to zero and fault.
//
do not initialize { section .noinit };
//
// Place the OTA CRC structure.
//
//place at start of CRC { readonly section .crc };
//
// Place the OTA Preamble structure.
//
//place at start of PREAMBLE { readonly section .preamble };
//
// Place the interrupt vectors.
//
place at start of FLASH { readonly section .intvec };
//
// Place the cca area at the end of flash.
//
place at start of FLASH_CCA { readonly section .cca };
//
// Place the commissioning parameter items.
//
place at start of CP_IEEE { readonly section IEEE_ADDRESS_SPACE };
place at start of CP_DEPK { readonly section DEV_PRIVATE_KEY_ADDRESS_SPACE };
place at start of CP_CAPK { readonly section CA_PUBLIC_KEY_ADDRESS_SPACE };
place at start of CP_IMPC { readonly section IMPLICIT_CERTIFICATE_ADDRESS_SPACE };
//
// Place the remainder of the read-only items into flash.
//
place in FLASH { readonly };
//
// Place the RAM vector table at the start of SRAM.
//
place at start of SRAM { section VTABLE };
//
// Place all read/write items into SRAM.
//
place in SRAM { readwrite, block HEAP };
//
// Place the ledger page, if it's defined
//
//place at start of LEDGER_PAGE { section .ledger };
//do not initialize { section .ledger };
//
// Place the bootloader page, if it's defined startup_ewarm
//
//place at start of BOOTLOADER_PAGE { section .bootloader };