This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请提供测试设备,被测板子和射频寄存器配置信息。频谱仪设置的是 Maximum Hold 吗?
测试仪器:R&S FSW .2Hz~26.5GHz
被测试板子是自己做的(后来发现Exposed die attach pad没有接地,是否这原因?)
寄存器配置:
{CC1101_PKTLEN, 13},
{CC1101_ADDR, 0X09},
{CC1101_PKTCTRL1, 0X43},
{CC1101_SYNC1, 0x87},
{CC1101_SYNC0, 0x99},
{CC1101_IOCFG0, 0x06},
{CC1101_FIFOTHR, 0x47},
{CC1101_PKTCTRL0, 0x05},
{CC1101_CHANNR, 0x01},
{CC1101_FSCTRL1, 0x06},
{CC1101_FREQ2, 0x0c},
{CC1101_FREQ1, 0x1d},
{CC1101_FREQ0, 0x89},
{CC1101_MDMCFG4, 0xF6},
{CC1101_MDMCFG3, 0x43},
{CC1101_MDMCFG2, 0x13},
{CC1101_DEVIATN, 0x15},
{CC1101_MCSM0, 0x18},
{CC1101_FOCCFG, 0x16},
{CC1101_WORCTRL, 0xFB},
{CC1101_FSCAL3, 0xE9},
{CC1101_FSCAL2, 0x2A},
{CC1101_FSCAL1, 0x00},
{CC1101_FSCAL0, 0x1F},
{CC1101_TEST2, 0x81},
{CC1101_TEST1, 0x35},
{CC1101_MCSM1, 0x3B},
频谱仪设置正确,用在另一个买的板子上是正常的(相同的程序),如下图:
您好,请问如何配置模块进入连续发载波的模式进行发射信号呢?我需要测试CC115L模块的发射功率。用频谱仪看波形和功率值。您那边能否提供相关寄存器的参考?谢谢!