This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101寄存器设置

Other Parts Discussed in Thread: CC1101

请问CC1101的寄存器MCSM0设置为0x08还是0x18?这2种设置分别适用于什么情况?

  • FS_AUTOCAL[1:0] 0 (00) R/W Automatically calibrate when going to RX or TX, or back to IDLE Setting When to perform automatic calibration

    0 (00) Never (manually calibrate using SCAL strobe)

    1 (01) When going from IDLE to RX or TX (or FSTXON)

     

    设置方式关键看你需不需要自动进行频率校准。