请教一下,国外免费的射频频段有哪些?除了2.4G。有相关的法律法规吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISM频段(Industrial Scientific Medical Band),就是各國挪出某一段頻段主要開放給工业,科学和医学機構使用。应用这些频段无需许可证或費用,只需要遵守一定的发射功率(一般低于1W),并且不要对其它频段造成干扰即可。ISM频段在各国的规定并不统一。如在美国有三个频段902-928 MHz、2400-2484.5 MHz及5725-5850 MHz,而在欧洲900MHz的频段则有部份用于GSM通信。而2.4GHz为各国共同的ISM频段。因此无线局域网(IEEE 802.11b/IEEE 802.11g),蓝牙,ZigBee等无线网络,均可工作在2.4GHz频段上。
ITU-R 指定的ISM频段如下:
| 频率范围 | 中心频率 | 可用性 |
|---|---|---|
| 6.765–6.795 MHz | 6.780 MHz | |
| 13.553–13.567 MHz | 13.560 MHz | |
| 26.957–27.283 MHz | 27.120 MHz | |
| 40.66–40.70 MHz | 40.68 MHz | |
| 433.05–434.79 MHz | 433.92 MHz | 仅限ITU Region 1 |
| 902–928 MHz | 915 MHz | 仅限ITU Region 2 |
| 2.400–2.500 GHz | 2.450 GHz | |
| 5.725–5.875 GHz | 5.800 GHz | |
| 24–24.25 GHz | 24.125 GHz | |
| 61–61.5 GHz | 61.25 GHz | |
| 122–123 GHz | 122.5 GHz | |
| 244–246 GHz | 245 GHz |
国际电盟网站http://www.itu.int/zh/ITU-R/