This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1354R10: 芯片的应用问题

Part Number: CC1354R10
Other Parts Discussed in Thread: CC1310

1、CC1310、CC1354使用时应该注意什么问题?
2、CC1354 400MHZ 规格书中一直不明示使用,请帮忙问一下TI公司是否有原因,我们使
用400M是否可以。我们使用CC1352用于中国物联网470-510MHz的有关公开资料说明,利用其中的400MHz设计TxRx电路是否合理?
3、温度信号从DIO_9\10\11进入是否可以?
4、48M、32.768KHZ两个晶振使用是否有特殊要求,这两个晶振有什么需要注意的地方?比如是否可以用用不同类型的晶振以及优缺点是什么?
5、编程时TCK\TMS\TDI\TDO都要用,规格书上只用了两个,为什么?
6、DIO_5\6\7有强驱动能力,有没有具体的解析?
7、CC1310、CC1354布线时需要注意哪些抗干扰问题。请提供有关layout的参考设计。
8、RX_TX的功能能不能具体分析一下,能够调用多个频段分别完成不同的上行和下行数据通信吗?
9、2.4G的输入分为正负端,在使用时应该注意什么?
10、天线有没有什么推荐的,使用时应该注意什么?
11、2.4G和400M同时使用时应该注意什么?
12、CC1354静态电流和动态电流是多少?
13、2.4G与400MHZ两个滤波通道有没有特别需要注意的地方?
14、帮忙申请提供CC1310、CC1354及周边元件的样品,
15.、CC1310、CC1354 是否可以控制信号和传输信号同步,当前控制信号和传输信息是用开发来切换的,换句话说,是否可以实现类似双工的传输方式,怎么样实现?
16.、CC1310,CC1354的12-bit SAR ADC, 200ksps, 8 channels 是指的 DIO 23 -30吗?
17、 CC310 CC354可否用户设置任务的优先级别吗?主要目的是保障控制信令和时间同步的信息的及时响应
18. 请尽可能完整提供有关cc1310 cc1354 有关参考电路设计和layout参考以及其它设计注意事项的资料