This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7970直接模式1和SOF EOF 10个etu

Other Parts Discussed in Thread: TRF7970A

TI的工程师们,我的一个项目准备采用TRF7970A进行无线研发,但是目前碰到了两个问题(如下),请工程师给予正确解答!

1,TRF7970在并行模式下如何进入直接模式1?在某些非标准协议中,能否采用直接模式0发送,采用直接模式1进行接收数据,如何进行设置?

2,TRF7970在14443B协议下,通过写02寄存器(ISO14443B TX 选项)0x00,确定SOF、EOF的时间宽度为SOF、EOF宽度为10个etu,但是在通过示波器观察,SOF、EOF的宽度有时候是10个etu,有时候是11个etu,有时候是介于二者之间的不定值,这种情况为什么?

谢谢!!!