This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SimpleProfile_SetParameter发送正常 但是GATT_Notification发送数据不对,求助!新版出现问题。

我使用

SimpleProfile_SetParameter( SIMPLEPROFILE_CHAR6,20,&databuf[sendok]);  

主机可以正确接受,如果主机(我使用的安卓BLE读写器),打开通知情况下,可以正确收到数据信息,能显示Notification,同时对数据进行读取都可以。

但是我只用GATT_Notification时,只能收到乱码,不是我真实发送的数据,但是数据长度是正确的,就是不是我实际发送的数据,代码如下:

static attHandleValueNoti_t pReport ;//声明attHandleValueNoti_t这个结构体
uint16 noti_cHandle; //存放handle
pReport.handle = simpleProfileAttrTbl[18].handle;//读取notification对应的handle
GAPRole_GetParameter( 0x30E, &noti_cHandle);//获取Connection Handle
pReport.len = 4;//数据长度
pReport.pValue[0] = 0x33;//赋值
pReport.pValue[1] = 0x34;//赋值
pReport.pValue[2] = 0x35;//赋值
pReport.pValue[3] = 0x36;//赋值
GATT_Notification(noti_cHandle,&pReport,FALSE);

下面附上我自己修改的simpleGATTprofile.c

我之前用1.3的时候没有这个问题,但是升级到最新版本发现这个问题,请问我是哪里有不对的地方,谢谢指教,调试了几天了,无解呢。。。

我目前使用GATT_Notification对attHandleValueNoti_t进行通知的时候, GATT_Notification并没有把结构体的pValue数据发送,但是进不去函数

所以现在无解了,请TI支持,万分感谢!

现在使用的版本是BLE-CC254x-1.4.1.43908