请问CC2530,不加PA放大,通信距主要是受什么所限制,是天线还是布板呢?
还有zigbee组网通信的时候,听说数据传递的跳转次数也有限制,不知道这个又是受什么限制的,主要是协议和通信数据长度所决定
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知你下的是哪个设计。一般情况下,在你下载的RD文件里面有一个readme文件。
相应的板材参数里面就有。
BR.AZ
一个叫 imported CC2530EM-discrete-1-3-1.PRJPCB的文件,没看到readme,不知道在哪里有下载你说的那个文件呢
你那个我还真不知道是哪一个:-)
你参考一下这个参考设计:http://www.ti.com/tool/CC2530EM?keyMatch=cc2530em%20rd&tisearch=Search-EN-Everything
http://www.ti.com/lit/zip/swrc144a
PCB DESCRIPTION: 2 LAYER PCB 0.8 MM Nominal thickness with 35um Cu in each layer
Dielectric constant for FR4 is 4.5
Dimensions in manufacturing files are in mils (0.001 inch)
DOUBLE SIDE SOLDER MASK,
DOUBLE SIDE SILKSCREEN,
8 MIL MIN TRACE WIDTH AND 8 MIL MIN ISOLATION.