This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC430接收中断出错

Other Parts Discussed in Thread: CC430F5137, CC1101

最近用CC430F5137做了两块实验板,实现数据收发,接收端接收到数据后,串口发送,在pc端利用串口助手查看数据。

现在的问题是,数据接收一段时间后,程序就死了,看着像是进不去接收中断了,请问有人有相关的经验指点一下吗??

具体的程序如下:

#define  PACKET_LEN         (0x06)     // PACKET_LEN <= 61
#define  CRC_LQI_IDX        (PACKET_LEN+1)  // Index of appended LQI, checksum
#define  CRC_OK             (BIT7)          // CRC_OK bit
#define  PATABLE_VAL        (0xC6)          // 10 dBm output
#define CPU_F   ((double)32768)
#define delay_ms(x)     __delay_cycles((long)(CPU_F*(double)x/1000.0))
extern RF_SETTINGS rfSettings;
RF_SETTINGS rfSettings = {
    0x06,   // FSCTRL1   Frequency synthesizer control.//
    0x00,   // FSCTRL0   Frequency synthesizer control.
    0x10,   // FREQ2     Frequency control word, high byte.//
    0xA7,   // FREQ1     Frequency control word, middle byte.//
    0x62,   // FREQ0     Frequency control word, low byte.//
    0xCA,   // MDMCFG4   Modem configuration.//
    0x83,   // MDMCFG3   Modem configuration.//
    0x13,   // MDMCFG2   Modem configuration.//
    0x22,   // MDMCFG1   Modem configuration.
    0xF8,   // MDMCFG0   Modem configuration.
    0x00,   // CHANNR    Channel number.//
    0x34,   // DEVIATN   Modem deviation setting (when FSK modulation is enabled).//
    0x56,   // FREND1    Front end RX configuration.
    0x10,   // FREND0    Front end TX configuration.
    0x10,   // MCSM0     Main Radio Control State Machine configuration.//
    0x16,   // FOCCFG    Frequency Offset Compensation Configuration.//
    0x6C,   // BSCFG     Bit synchronization Configuration.//
    0x43,   // AGCCTRL2  AGC control.
    0x40,   // AGCCTRL1  AGC control.
    0x91,   // AGCCTRL0  AGC control.
    0xE9,   // FSCAL3    Frequency synthesizer calibration.//
    0x2A,   // FSCAL2    Frequency synthesizer calibration.//
    0x00,   // FSCAL1    Frequency synthesizer calibration.//
    0x1F,   // FSCAL0    Frequency synthesizer calibration.//
    0x59,   // FSTEST    Frequency synthesizer calibration.
    0x81,   // TEST2     Various test settings.//
    0x35,   // TEST1     Various test settings.//
    0x09,   // TEST0     Various test settings.//
    0x47,   // FIFOTHR   RXFIFO and TXFIFO thresholds.//
    0x29,   // IOCFG2    GDO2 output pin configuration.
    0x06,   // IOCFG0    GDO0 output pin configuration. Refer to SmartRF Studio User Manual for detailed pseudo register explanation.
    0x04,   // PKTCTRL1  Packet automation control.
    0x04,   // PKTCTRL0  Packet automation control.
    0x00,   // ADDR      Device address.
    0x06    // PKTLEN    Packet length.
};
unsigned char PacketReceived;
unsigned char Receiving = 0;
unsigned char RxBuffer[PACKET_LEN+2];
unsigned char RxBufferLength = 0;
unsigned char SlaveStepInfo[PACKET_LEN];
void main( void )

  // Stop watchdog timer to prevent time out reset
  WDTCTL = WDTPW + WDTHOLD;
  // Increase PMMCOREV level to 2 for proper radio operation
  SetVCore(2);                           
 
  ResetRadioCore();    
  InitRadio();
  InitIO();
  InitUART();
 
  ReceiveOn();
  Receiving = 1;
 
  PacketReceived = 0;
   
  while (1)
  {
      _EINT();
     
      __no_operation();
        
      if(PacketReceived)
      {
        P3OUT |= BIT4;
        delay_ms(1000);
       
        for( unsigned char i = 0; i < PACKET_LEN; i++)
        {
          SlaveStepInfo[i] = RxBuffer[i];
         
        }
       
        for(unsigned char j = 0; j < PACKET_LEN; j++)
        {
          while (!(UCA0IFG&UCTXIFG));                   // USCI_A0 TX buffer ready?
          UCA0TXBUF = SlaveStepInfo[j];                 // TX -> RXed character
        }  
       
        delay_ms(1000);
        P3OUT &= ~BIT4;
       
        PacketReceived = 0;
        Receiving = 1;
        ReceiveOn();
      }
  }  
}
void InitIO(void)
{
 // Initialize Port J
  PJOUT = 0x00;
  PJDIR = 0xFF;
  // Set up LEDs
  P3OUT &= ~(BIT4+BIT5);
  P3DIR |= BIT4+BIT5;
}
void InitRadio(void)
{
  // Set the High-Power Mode Request Enable bit so LPM3 can be entered
  // with active radio enabled
  PMMCTL0_H = 0xA5;
  PMMCTL0_L |= PMMHPMRE_L;
  PMMCTL0_H = 0x00;
 
  WriteRfSettings(&rfSettings);
 
  WriteSinglePATable(PATABLE_VAL);
}
void ReceiveOn(void)

  RF1AIES |= BIT9;                          // Falling edge of RFIFG9
  RF1AIFG &= ~BIT9;                         // Clear a pending interrupt
  RF1AIE  |= BIT9;                          // Enable the interrupt
 
  // Radio is in IDLE following a TX, so strobe SRX to enter Receive Mode
  Strobe( RF_SRX );                     
}
void ReceiveOff(void)
{
  RF1AIE &= ~BIT9;                          // Disable RX interrupts
  RF1AIFG &= ~BIT9;                         // Clear pending IFG
  // It is possible that ReceiveOff is called while radio is receiving a packet.
  // Therefore, it is necessary to flush the RX FIFO after issuing IDLE strobe
  // such that the RXFIFO is empty prior to receiving a packet.
  Strobe( RF_SIDLE );
  Strobe( RF_SFRX  );                      
}
#pragma vector=CC1101_VECTOR
__interrupt void CC1101_ISR(void)
{
  switch(__even_in_range(RF1AIV,32))        // Prioritizing Radio Core Interrupt
  {
    case  0: break;                         // No RF core interrupt pending                                           
    case  2: break;                         // RFIFG0
    case  4: break;                         // RFIFG1
    case  6: break;                         // RFIFG2
    case  8: break;                         // RFIFG3
    case 10: break;                         // RFIFG4
    case 12: break;                         // RFIFG5
    case 14: break;                         // RFIFG6         
    case 16: break;                         // RFIFG7
    case 18: break;                         // RFIFG8
    case 20:                                // RFIFG9
      if(Receiving)       // RX end of packet
      {
        RF1AIE &= ~BIT9;                          // Disable RX interrupts
        RF1AIFG &= ~BIT9;                         // Clear pending IFG
       
        // Read the length byte from the FIFO      
        RxBufferLength = ReadSingleReg( RXBYTES );              
        ReadBurstReg(RF_RXFIFORD, RxBuffer, RxBufferLength);
       
        // Stop here to see contents of RxBuffer
        __no_operation();     
       
        // Check the CRC results
        if(RxBuffer[CRC_LQI_IDX] & CRC_OK) 
        PacketReceived = 1;                 // Packet Received Sucessfully 
       
        Receiving = 0;
        Strobe( RF_SIDLE );
        Strobe( RF_SFRX  );  
       
      }
      break;
    case 22: break;                         // RFIFG10
    case 24: break;                         // RFIFG11
    case 26: break;                         // RFIFG12
    case 28: break;                         // RFIFG13
    case 30: break;                         // RFIFG14
    case 32: break;                         // RFIFG15
  } 
  __bic_SR_register_on_exit(LPM3_bits);    
}