A、B两种板子,每种板子做了几块,A板面积38mm*70mm,B板面积50mm*130mm。
315MHz。
B板发送,另一块B收接收正常,没有误码;
B板发送,另一块A板接收,误码率很高,约有40%;
A板发送,另一块B板接收正常,几乎没有误码;
A板发送,另一块A板几乎收不到数据;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
A、B两种板子,每种板子做了几块,A板面积38mm*70mm,B板面积50mm*130mm。
315MHz。
B板发送,另一块B收接收正常,没有误码;
B板发送,另一块A板接收,误码率很高,约有40%;
A板发送,另一块B板接收正常,几乎没有误码;
A板发送,另一块A板几乎收不到数据;
PCB Layout有很大关系,微带线Componet值是否有更换?
思路就是先看传导,再看天线
建议按下面顺序测试和 Debug:
先测测晶振的频率误差;
再测发送功率;
灵敏度不太好测,最后有需要再测试。
CC1101寄存器的配置如下,两种板子配置相同。其它寄存器为默认值
typedef struct S_RF_SETTINGS
{
uint8_t FSCTRL1; // Frequency synthesizer control.
uint8_t FSCTRL0; // Frequency synthesizer control.
uint8_t FREQ2; // Frequency control word, high uint8_t.
uint8_t FREQ1; // Frequency control word, middle uint8_t.
uint8_t FREQ0; // Frequency control word, low uint8_t.
uint8_t MDMCFG4; // Modem configuration.
uint8_t MDMCFG3; // Modem configuration.
uint8_t MDMCFG2; // Modem configuration.
uint8_t MDMCFG1; // Modem configuration.
uint8_t MDMCFG0; // Modem configuration.
uint8_t CHANNR; // Channel number.
uint8_t DEVIATN; // Modem deviation setting (when FSK modulation is enabled).
uint8_t FREND1; // Front end RX configuration.
uint8_t FREND0; // Front end RX configuration.
uint8_t MCSM0; // Main Radio Control State Machine configuration.
uint8_t FOCCFG; // Frequency Offset Compensation Configuration.
uint8_t BSCFG; // Bit synchronization Configuration.
uint8_t AGCCTRL2; // AGC control.
uint8_t AGCCTRL1; // AGC control.
uint8_t AGCCTRL0; // AGC control.
uint8_t FSCAL3; // Frequency synthesizer calibration.
uint8_t FSCAL2; // Frequency synthesizer calibration.
uint8_t FSCAL1; // Frequency synthesizer calibration.
uint8_t FSCAL0; // Frequency synthesizer calibration.
uint8_t FSTEST; // Frequency synthesizer calibration control
uint8_t TEST2; // Various test settings.
uint8_t TEST1; // Various test settings.
uint8_t TEST0; // Various test settings.
uint8_t IOCFG2; // GDO2 output pin configuration
uint8_t IOCFG0; // GDO0 output pin configuration
uint8_t PKTCTRL1; // Packet automation control.
uint8_t PKTCTRL0; // Packet automation control.
uint8_t ADDR; // Device address.
uint8_t PKTLEN; // Packet length.
uint8_t WORCTRL;
} RF_SETTINGS;
const RF_SETTINGS rfSettings = {
0x08, // FSCTRL1:IF frequency of 381kHz
0x00, // FSCTRL0:
0x0C, // FREQ2 Frequency control word, high byte.
0x1D, // FREQ1 Frequency control word, middle byte.
0x89, // FREQ0 Frequency control word, low byte, RF Frequency=315MHz
0x5B, // MDMCFG4 滤波带宽 kHz
0xF8, // MDMCFG3 波特率=100bps
0x13, // MDMCFG2 30/32 sync word bits detected、GFSK调制模式、Enable digital DC blocking filter
0x22, // MDMCFG1 FEC功能禁止、4bytes preamble、2 bit exponent of channel spacing
0xF8, // MDMCFG0 channel spacing = (65536/262144)*(256+0XF8)*2^2=199.951 kHz
0x00, // CHANNR Channel number.
0x47, // DEVIATN(when FSK modulation is enabled)
0xB6, // FREND1:
0x10, // FREND0:选择PATABLE[0]
0x18, // MCSM0: sleep模式下XOSC无效;
0x1D, // FOCCFG Frequency Offset Compensation Configuration.
0x1C, // BSCFG Bit synchronization Configuration.
0xC7, // AGCCTRL2 AGC control.
0x00, // AGCCTRL1 AGC control.
0xB2, // AGCCTRL0 AGC control.
0xEA, // FSCAL3 Frequency synthesizer calibration.
0x2A, // FSCAL2 Frequency synthesizer calibration.
0x00, // FSCAL1 Frequency synthesizer calibration.
0x1F, // FSCAL0 Frequency synthesizer calibration.
0x59, // FSTEST Frequency synthesizer calibration.
0x88, // TEST2 Various test settings.
0x31, // TEST1 Various test settings.
0x0B, // TEST0 Various test settings.
0x29, // IOCFG2 GDO2 output pin configuration.
0x06, // IOCFG0:a sync word has been transmitted 、a complete packet has been transmitted
0x24, // PKTCTRL1:A threshold of 4PQT 无地址检测校验, no broadcast、APPEND_STATUS包含
0x45, // PKTCTRL0:包长不固定,由sync字节后的Packet length字节确定、CRC使能、Whitening on
0x00, // ADDR:Device address
0xFF, // PKTLEN:最大包长度为16,收到的包长度超过16则丢弃
0xFB // WORCTRL
};
我没有按照DN015执行频率校正