This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

提高CC1101通讯距离和稳定性



      现在做的一样项目:按照TI官网上的参考硬件设计,由于通讯距离不够(要求200m,测试中100m就出现通讯不稳定),所以改板时在接收机上做了一个LNA(实际就是RF transistor),理论值是23DB,从接收机的RSSI监测的实际值来看也有15DB以上。参数设计如下:data rata:250kbps、devation是127khz、RX BW是541khz,发射机天线采用1.5dbi的弹簧天线,接收机采用6dbi的吸盘天线。

      经过几天的测试发现,带LNA的接收机与不带LNA的接收机相比。带LNA的接收机监测的RSSI虽然提高有15-20DB的样子,但是实际接收效果跟不带LNA的差不多,因为带LNA的接收机在-70DB左右就出现接收困难的问题。而不带LNA的接收机虽然监测到的RSSI较差,但是在-85DB的时候才出现接收困难的情况。这样看来其实两者的接收效果其实差不多,都满足不了需求。

      请问各位大侠,就目前的情况来看,我应该如何优化?