This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: 更新固件错误

Part Number: LAUNCHXL-CC1310


In the case that the XDS110 fails to enumerate as a USB device, you can attempt restore functionality by updating the firmware using a JTAG connection. Contact your vendor for details on how to attach a JTAG cable and for what programmer tool you should use. Perform the following steps to restore the firmware: 1. Connect the flash tool to the XDS110’s CPU using JTAG connection. 2. Use the flash tool to erase the entire flash of the XDS110. 3. Flash the boot_loader.bin file to address 0x0000. 4. Power cycle the XDS110 (unplug and re-plug it into the USB port). 5. Use the xdsdfu utility to update the firmware as detailed above. The firmware is now updated, and the XDS110 debug probe should be ready to use.

不知道应该如何处理