Part Number: TPS54362-HT
您好!在设计中遇到TPS54362-HT无输出。输入24V,输出12V。刚开始有输出,但是功耗较大,输入侧有80MA电流,芯片发烫。加载或过一会儿,无输出了。输入侧只有3MA电流。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54362-HT
您好!在设计中遇到TPS54362-HT无输出。输入24V,输出12V。刚开始有输出,但是功耗较大,输入侧有80MA电流,芯片发烫。加载或过一会儿,无输出了。输入侧只有3MA电流。
重新上电以后还是没有输出,输入侧只有3MA电流。输入电压24V正常,EN引脚是经过分压的,大概十几伏左右。boot引脚有1.6V.其他引脚几乎没有输出。
TPS54362-HT输出不稳定.带载不足。
可能有下面的原因。
你排查下。
不合理的布局走线可能会产生寄生电感、电容和电阻,导致输出振荡。确保关键路径的电感和电容最小化。
Boot电容不足:在轻载情况下,Boot电容可能不足以维持正常工作。
如果芯片在带载后过热,可能会触发保护机制,导致输出不稳定。