Part Number: CC1310
void Timer0_Callback(void)
{
TimerIntClear(GPT0_BASE, TIMER_TIMA_TIMEOUT);//清空中断
GPIO_toggle(Board_GPIO_LED0);
}
void Timer0_Init(void)
{
// Power on the TIMER0 peripheral
PRCMPeripheralRunEnable(PRCM_PERIPH_TIMER0);
TimerDisable(GPT0_BASE, TIMER_A);
TimerConfigure(GPT0_BASE, TIMER_CFG_SPLIT_PAIR |TIMER_CFG_A_PERIODIC_UP);
TimerLoadSet(GPT0_BASE, TIMER_A, 200);
TimerPrescaleSet(GPT0_BASE, TIMER_A, 48-1);//实际分频值加1
//TimerIntervalLoadMode(GPT0_BASE, TIMER_A, TIMER_INTERVALLOAD_NEXTCYCLE);//更新模式:在下个时钟周期
TimerIntRegister(GPT0_BASE, TIMER_A, Timer0_Callback);
TimerIntEnable(GPT0_BASE, TIMER_TIMA_TIMEOUT);
TimerIntClear(GPT0_BASE, TIMER_TIMA_TIMEOUT);//清空中断
TimerEnable(GPT0_BASE, TIMER_A);
}
请问这段代码定时器时间视乎不起作用,一直是63.9ms,改LOAD值定时时间也不变,不知是哪的问题。